Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog New technique ‘amps’ potential for gallium nitride electronics
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ZeroSizeObject
  • Date Created: 3 Feb 2011 7:49 PM Date Created
  • Views 776 views
  • Likes 0 likes
  • Comments 0 comments
  • gallium_nitride
  • research
  • ic
  • materials
  • embedded
  • silicon
Related
Recommended

New technique ‘amps’ potential for gallium nitride electronics

ZeroSizeObject
ZeroSizeObject
3 Feb 2011
image
Gallium nitride material holds promise for emerging high-power devices that are more energy efficient than existing technologies, but these GaN devices traditionally break down when exposed to high voltages. Now researchers at North Carolina State University have solved the problem, introducing a buffer that allows the GaN devices to handle 10 times greater power. Previous research into developing high power GaN devices ran into obstacles, because large electric fields were created at specific points on the devices’ edge when high voltages were applied, effectively destroying the devices. NC State researchers have addressed the problem by implanting a buffer made of the element argon at the edges of GaN devices. The buffer spreads out the electric field, allowing the device to handle much higher voltages. The researchers tested the new technique on Schottky diodes and found that the argon implant allowed the GaN diodes to handle almost seven times higher voltages. The diodes that did not have the argon implant broke down when exposed to approximately 250 volts. The diodes with the argon implant could handle up to 1,650 volts before breaking down. “By improving the breakdown voltage from 250 volts to 1,650 volts, we can reduce the electrical resistance of these devices a hundredfold. That reduction in resistance means that these devices can handle ten times as much power,” said Dr. Jay Baliga, Distinguished University Professor of Electrical and Computer Engineering at NC State.

Zero