Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Noise-canceling kennel for scaredy-cats and dogs
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 27 Dec 2018 7:31 PM Date Created
  • Views 1880 views
  • Likes 7 likes
  • Comments 3 comments
  • ford
  • sound canceling
  • prototype
  • pets
  • cabeatwell
  • sound
  • innovation
Related
Recommended

Noise-canceling kennel for scaredy-cats and dogs

Catwell
Catwell
27 Dec 2018

image

The prototype has lots of potential for pets to hide from loud noise. The noise-canceling kennel is only a prototype, but it has a lot of potential in the future. (Credit: Lyn West, Ford of Europe)


Many pet owners worry about the nightmarish sounds left behind by fireworks and the impact it has on their pets and for good reason too. I had a dog once that was frightened of fireworks and thunderstorms, so I sympathize. We all know, their hearing is a lot more sensitive than humans, so it's not a surprise that most pets start showing signs of fear and distress when fireworks start popping.

 

A solution to help ease dog's distress/fear or eliminate it completely during a display of fireworks would be to use the noise-canceling kennel, from Ford, that uses similar technology found in cars and headphones.

 

Microphones inside the kennel detect the sound of fireworks and once that happens, a built-in audio system emits opposing frequencies. That causes the noise to be canceled out completely or lessened significantly. The kennel also uses high-density cork in its design to carry out the sound-proofing. This is only a prototype for now, but it bodes well for the future for pet owners and their pets.

 

This idea was inspired by the noise-canceling technology found in the Edge SUV that allows for a much quieter experience in their car journeys for drivers and passengers. The noise is canceled out when microphones in the SUV pick up high levels of noise from the engine or transmission and counteracts it by using opposing sound waves from the audio system.

 

The noise-canceling kennel is just a prototype for now, but it belongs to a series of initiatives called interventions which applies automotive technology to help solve everyday problems.

 

I could use something like this in office situations. Especially open office layouts.

 

 

This video is unavailable.
You don't have permission to edit metadata of this video.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • jdlui
    jdlui over 7 years ago +1
    Interesting idea. I'm wondering how effective this is for dogs, since their hearing is more sensitive than ours and covers a wider frequency spectrum. I'm wondering if the anti-node sounds that the system…
  • Gough Lui
    Gough Lui over 7 years ago +1
    I like the redundancy in the tagline: The prototype has lots of potential for pets to hide from loud noise. The noise-canceling kennel is only a prototype , but it has a lot of potential in the future…
  • anupash.1002
    anupash.1002 over 7 years ago

    Its a good idea. Can also be used for human babies.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago

    I like the redundancy in the tagline:

    The prototype has lots of potential for pets to hide from loud noise. The noise-canceling kennel is only a prototype, but it has a lot of potential in the future.

     

    or in other words ...

    The noise-cancelling kennel is a prototype which shows potential in allowing pets to hide from loud noise.

     

    Which just seems like fancy words for someone's concept idea that hasn't really been well tested and instead is more of an advertisement for Ford's vehicles that incorporate cabin-based noise cancelling technologies. Instead, the whole association with pets is more of an appeal to pet owners especially around the holiday season. Yay for advertising.

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jdlui
    jdlui over 7 years ago

    Interesting idea.

    I'm wondering how effective this is for dogs, since their hearing is more sensitive than ours and covers a wider frequency spectrum. I'm wondering if the anti-node sounds that the system creates would cause any discomfort to the animal?