Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog RISC-V Becomes the New Standard In Devices
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 3 May 2023 9:55 PM Date Created
  • Views 1161 views
  • Likes 10 likes
  • Comments 1 comment
  • coding
  • risc
  • programming
  • cabeatwell
  • risc-v
  • mcu
  • university
  • innovation
Related
Recommended

RISC-V Becomes the New Standard In Devices

Catwell
Catwell
3 May 2023

image

Devices, such as a laptop, have an instruction set architecture, and the RISC-V is becoming a new standard. (Image Credit: Enkin_Akyurt/pixabay)

Both the x86 and ARM ISAs (Instruction Set Articheture) are commonly found in varying devices. However, these have high costs due to licensing fees that allow the company to integrate them. RISC-V (Reduced Instruction Set Computer) has recently joined the stage and could give developers more creativity. Plus, it has the potential to help introduce futuristic technologies such as self-driving cars and quantum computers. RISC-V was first developed in 2010 at the University of California, Berkeley. During that time, professors were exploring new methods to teach computer architecture and design to students. 

When RISC-V didn't exist, academic computer scientists would create computer instruction sets for research projects. Doing so allowed them to avoid creative, financial, and legal limitations. Over the past few years, RISC-V has emerged as a royalty-free set for inventors to use on their terms. 

Google, a RISC-V international member, plans on integrating the standard into Android and other devices. Intel has also joined the effort even though it owns the x86 ISA. Qualcomm announced it delivered 650 million RISC-V cores for IoT, automotive, mobile, and extended reality applications. 

Additionally, tech companies can produce new instructions, which is exciting for those that purchase ISA licensing. Western Digital became one of the first to integrate RISC-V into a commercial device. Then, in 2019, the company said it would start creating instructions for faster, more efficient hard drives. 

Other than making devices last longer, RISC-V can also be used in cryptocurrency, quantum computing, AI, and machine learning. Plenty of computer power must be used, and that tech needs to run on various processors simultaneously. That's because computer processor improvements may not be able to keep pace with advanced research. RISC-V can potentially speed up self-driving car progress. For instance, Ventana develops RISC-V chips designed for futuristic cars to handle heavy amounts of data while driving humans. 

However, many challenges need to be considered before proceeding. For one thing, the tech is still new, so technologies that would be made of a RISC-V system must be developed first. So far, companies have begun developing supporting components for those systems.

Have a story tip? Message me at: http://twitter.com/Cabe_Atwell

  • Sign in to reply
Parents
  • embeddedguy
    embeddedguy over 3 years ago

    A good comprehensive article BTW companies will have to create software support for RISK-V mainly because other hardware protocols and stuff work ideal in both. 
    I read an article where Nordic semiconductors will also have RISK-V processors in the upcoming nRF54 series. Interesting is also that how this multiple cores communicate with each other over some protocols.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • embeddedguy
    embeddedguy over 3 years ago

    A good comprehensive article BTW companies will have to create software support for RISK-V mainly because other hardware protocols and stuff work ideal in both. 
    I read an article where Nordic semiconductors will also have RISK-V processors in the upcoming nRF54 series. Interesting is also that how this multiple cores communicate with each other over some protocols.