Topographic image of Bi2Sr2CaCu2O8+δ, showing crystal supermodulation. (Image Credit: Science (2026))
Scientists from Leiden, Munich, and Utrecht conducted a study to better understand high-temperature superconductors. This may help scientists discover materials that can conduct electricity with zero resistance at everyday temperatures.
Scanning tunneling microscopy and shot-noise measurements enabled them to investigate Bi₂Sr₂CaCu₂O₈₊δ, a cuprate high-temperature superconductor. Samples with various superconducting transition temperatures, such as underdoped, optimally doped, and overdoped materials were then examined.
In the paper, the team says that, in a cuprate high-temperature superconductor, electron pairs may persist at room temperature. This is higher than the temperature at which the material becomes superconducting. Based on the finding, pairing electrons isn’t the only barrier. Each pair needs to behave coherently, which means moving in a coordinated collective state.
The team compared the energy associated with electron pairing to the material’s pseudogap energy. By doing so, this showed both energies match across samples with different superconducting transition temperatures. Since the pseudogap can persist up to room temperature, the team says that electron pairing may also persist there.
The researchers measured at cryogenic temperatures (360 mK to 4.3 K). More tests using gold and by applying magnetic fields allowed them to determine that the signal is associated with electron pairing, not equipment error.
Electricity is conducted from superconductors with no resistance. Most materials require extreme cooling. High-temperature cuprate superconductors function at cryogenic temperatures, making widespread use more challenging.
It’s essential for electrons to form Cooper pairs so that superconductivity will occur. And they must be phase coherent. Those processes happen together in conventional low-temperature superconductors. A key signal was a step-like increase in the effective charge measured via shot noise. This signal helped identify the energy at which pairing emerges.
Have a story tip? Message me here at element14.