Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Stanford Researchers Employ World’s Smallest Diamonds to Create Wires Only 3-Atoms Wide
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 2 Feb 2017 1:42 AM Date Created
  • Views 1393 views
  • Likes 1 like
  • Comments 3 comments
  • research
  • mit
  • on_campus
  • wire
  • cabeatwell
  • standford
  • university
  • innovation
Related
Recommended

Stanford Researchers Employ World’s Smallest Diamonds to Create Wires Only 3-Atoms Wide

Catwell
Catwell
2 Feb 2017

image

Standford and DOE researchers have created super-thin wires just three atoms wide using diamonds and assembling them Lego-style. (via Standford)

 

Researchers from Stanford University and the Department of Energy (DOE) have developed a way to use diamonds- tiny bits of diamonds, to create a wire that is only three atoms wide. The wires have the potential to be used in all sorts of applications, including electricity-generating fabrics, optoelectronic devices and crazy superconducting materials that won’t bleed electricity.

 

What’s more, the building process of the wires requires a new Lego-like assembling technique and begins with attaching a single sulfur atom to a small diamondoid (nano-diamond or carbon cage molecule), which is then dropped into a solution where the sulfur atom bonds with a copper ion. The bonding doesn’t stop there, as diamondoids (in this case adamantane) are extremely attracted to each other through what is known as van der Waals forces- the same force that allows geckos to stick to walls.

 

In the diamondoid’s case, the force makes them clump together similar to sugar crystals and as you might have guessed, self-assemble to create a wire structure, complete with a copper-ion core. Stanford grad student Fei Hua Li (the mind behind figuring out the diamondoid’s attractive properties) explains it this way- “Much like LEGO blocks, they only fit together in certain ways that are determined by their size and shape.” He went on to say, “The copper and sulfur atoms of each building block wound up in the middle, forming the conductive core of the wire, and the bulkier diamondoids wound up on the outside, forming the insulating shell.”

 

image

The basic building block of the nano-wire shows the copper/sulfur center being self-assembled by the attracting diamondoid outer shell.

 

Beyond using copper-ion based wires, the researchers also created them using other metals such as cadmium, zinc, iron and silver- all created using different solutions and with different cage molecules. What’s interesting is that each different build had similar material properties to some of those used in today’s technological applications.

 

For instance, the cadmium-based nano-wires had similar material properties to those used in optoelectronics such as LEDs, while the zinc-based wires are similar to those found in some solar panels and piezoelectric generators. The possibilities of using these wires for creating a host of new materials with electrical properties are almost endless, their development is still in its infancy but considering that they have virtually no electrical bleed, it will be exciting to see what they can be adapted for beyond just efficient electronics.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

 

  • Sign in to reply
  • DAB
    DAB over 9 years ago in reply to Catwell

    Not yet, we are completely updating the book and I am creating a new periodic table to better explain what is inside atoms and why they can be better manipulated.

     

    I have not even sat down to fully explore what I have learned over the last six months on chemistry and biology, but there are clearly exploitable capabilities.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 9 years ago in reply to DAB

    Can you link to your thoughts on the subject anywhere?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago

    Hi Cabe,

     

    I have been finding this type of interesting behavior exists in many atomic structures.

    Depending upon the specific crystal structures formed, the resulting atom formations support many different types of photon emissions at many wavelengths.

     

    This story supports many of the insights into atomic behavior based upon my new atomic model.

     

    DAB