Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Supercapacitor-powered Speaker Charges in Five Minutes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 7 Nov 2014 7:17 AM Date Created
  • Views 903 views
  • Likes 0 likes
  • Comments 2 comments
  • supercapacitor
  • ultracap
  • embedded
  • Design
  • supercap
  • cabeatwell
  • sound
  • crowd_funding
  • music
  • ultracapacitor
  • speaker
Related
Recommended

Supercapacitor-powered Speaker Charges in Five Minutes

Catwell
Catwell
7 Nov 2014

image

Blueshift Hydrogen (via Blueshift)

 

If you thought the ‘80s mobile boombox was out of style, guess again. Blueshift recently announced the launch of its portable, supercapacitor-powered, Bluetooth speaker, Hydrogen – your new best friend.

 

The Blueshift Hydrogen speaker is changing the nature of mobile devices. The portable Bluetooth speaker is powered by supercapacitors, and while it only takes five minutes to fully charge, the 4lb speaker can play for more than 4 hours at 80 percent volume. Connect it to your computer, cell phone, or any other Bluetooth-capable device and let the beat drop.

 

image

Inside the Hydrogen speaker (via Blueshift)

 

Blueshift’s Hydrogen sits at 9” x 8” x 4.” What it lacks in stature it makes up for in sound. The beach-friendly box speaker features a 3” full-range driver, Class-D amplifier and volume controls, housed in a bamboo shell – a wood which really vibrates well for music., All of the speaker’s parts are custom-made in America and the entire unit is plastic-free. The real secret, however, are the supercapacitors.

 

While batteries store chemical energy, supercapacitors house energy in the form of a physical, electric field. This allows for the technology to charge rapidly and remain extremely durable. For example, the supercapacitors that power the Hydrogen speaker charge in five minutes and are guaranteed to function at optimal energy levels for up to half a million charges. If the same technology is applied to mobile devices everywhere (or any electronic devices, for that matter), your local energy company would be very upset.

 

The Hydrogen speaker is open-source and includes a Bluetooth A2DP and 1/8” wired input, 1/8” cable and AC charger in the box. Blueshift claims that the Hydrogen speaker is built to last. All of the parts are easily replaceable and/or upgradeable and all of the parts, from the components to the bamboo shell itself, are durable. With this, since the project is open-source, Blueshift welcomes new upgrades and enhancements from consumers. While supercapacitors are still more expensive than traditional batteries, having a practical way to use the technology really opens the doors for makers to change the way we charge. 

Blueshift has designed a number of other speakers, currently on presale via Crowd Supply, including a subwoofer, entitled Iron Subwoofer, preamp and home sound system. All of the speakers feature bamboo and the signature Blueshift simplistic design. While the designs are open hardware, the retail versions are proprietary.

 

image

Blueshift Product Line (via Blueshift)

 

Blueshift is currently running a crowd-funding campaign via Crowd Supply. The Hydrogen speaker will retail for $400, but is on sale for early backers at $330. All of the company’s speakers are on presale, but the Hydrogen may be the best bang for your buck. Cool Material was quoted saying that the portable speaker might be the best deal in the market, when factoring charge time vs. playback.

 

The crowd funding campaign is open for two more weeks, so if you’re considering buying one, act now. Honestly, who couldn’t use a portable speaker? So, hurry and support their effort!


Sure, they’re wonderfully useful at morning board meetings, but they’re epically awesome on the beach. C’mon man. Drop that bass.


C

See more news at:

http://twitter.com/Cabe_Atwell

  • Sign in to reply
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    How do you keep a supeecapacitor from working like a capacitor and dumping it's whole load at one time?  I thought that's how they worked.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 11 years ago

    How do you keep a supeecapacitor from working like a capacitor and dumping it's whole load at one time?  I thought that's how they worked.