Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog This chip self-destructs on command in ten seconds
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 17 Sep 2015 6:52 PM Date Created
  • Views 3001 views
  • Likes 3 likes
  • Comments 12 comments
  • self_destructing_chip
  • destroy
  • security
  • xerox
  • cabeatwell
  • parc
  • innovation
Related
Recommended

This chip self-destructs on command in ten seconds

Catwell
Catwell
17 Sep 2015

image

Made out of Gorilla Glass, the chip obliterates itself. This new chip shatters into thousands of pieces under extreme stress. (via Xerox PARC, pic via IDG.tv)


I was just thinking, there has to be a way to store data that will self-destruct upon access. Seems we are close to it.

 

The latest development from Xerox PARC engineers is a device straight out of a James Bond film. The team has created a chip that can explode into bits on command as part of the Defense Advanced Research Projects Agency's (DARPA) Vanishing Programmable Resources project. How does the chip get this shattering effect? It was made using Gorilla Glass, supposed used for smart phone screens, instead of plastic and metal. The glass was then modified to become tempered glass under extreme stress, which will case it to easily disintegrated when triggered.

 

In a demonstration, the chip reached breaking point by heat. A small resistor heated up and the glass shattered into a ton of tiny pieces. Even after it broke, the small fragments continued to break into even smaller pieces for tens of seconds afterward.

 

Is the chip supposed to just look cool? Even though the result is awesome, the chip can actually be a great security measure. It could be used to store sensitive data like encryption keys and can shatter into so many pieces it becomes impossible to reconstruct it. It's a pretty intense way to deal with electronic security, but it's a viable option if it happens to fall into the wrong hands.

 

The self-destructible chip was demonstrated in all its glory at DARPA's Wait, What? Event in St. Louis last week.

 

“The applications we are interested in are data security and things like that,” said Gregory Whiting, a senior scientist at PARC in Palo Alto, California. “We really wanted to come up with a system that was very rapid and compatible with commercial electronics.”

 

With so much information being stored electronically, more and more companies are employing similar techniques for security. Similar technology is used for Snapchat, which lets users send images to friends for a short amount of time before the message can no longer be accessed. And Gmail recently introduced the “Undo Send” feature that allows people to cancel sent emails, but it's limited to 30 messages. Now, if only we could make our phones explode when they get stolen.

 

PARC is a Xeorx company that provides tech services, expertise, and intellectual property to various companies including Fortune 500 businesses, startups, and government agencies.


You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

C

See more news at:

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • Catwell
    Catwell over 11 years ago in reply to DAB +2
    I would imagine it's for planned destruction events. C
  • phoenixcomm
    phoenixcomm over 11 years ago in reply to Catwell +2
    Good morning, Mr Phelps, This tape will self-destruct in 10 seconds!!
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to phoenixcomm +2
    Warning! the atmospheric processor will self-destruct in 30 minutes ... Warning! the atmospheric processor will self-destruct in 29 minutes ... Warning! the atmospheric processor will self-destruct in…
Parents
  • mudz
    mudz over 10 years ago

    Oh I have this self destructible chip, I have only one copy of this 1 year of research data, very important data which I'm going to discuss within a group of people a secret meeting.. Here I have this chip sitting on the table and suddenly I accidently put my hot coffee cup on it.. Bammm..
    My point is, they need to come up with some other idea than the "rising temperature and shattering stuff".. No offence but Hey I can do that better at my home.. try to come up with something innovative with those expensive machines, research & Testing devices..

     

    mudz

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 10 years ago in reply to mudz

    Mudz...

     

    How about melting... As you access the data, it melts.

     

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mudz
    mudz over 10 years ago in reply to Catwell

    How about not breaking or melting anything? Just make tiny parallel processor(like in gpu) within the flash which when receiving a special command rewrites whole of the flash many times?
    So it can be reused!


    mudz

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 10 years ago in reply to mudz

    If it isn't destroyed completely... some way, some how... the data could get recovered.

     

    I think the key is time.   To re-write over enough times could take a while, depending on the size.

    So, imagine 1TB drive of super-secret spy data melts in 30 seconds... bad guys thwarted!

     

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Catwell
    Catwell over 10 years ago in reply to mudz

    If it isn't destroyed completely... some way, some how... the data could get recovered.

     

    I think the key is time.   To re-write over enough times could take a while, depending on the size.

    So, imagine 1TB drive of super-secret spy data melts in 30 seconds... bad guys thwarted!

     

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mudz
    mudz over 10 years ago in reply to Catwell

    That's why I said to use parallel processors(like in GPU).. every large bit/byte colony is attached to one cpu so that every flash bit can be rewrite within microseconds? Well, yes they need to write a new architecture for that but if they are going to so much of pain(making it on glass.. ahah) they can do that too.. I believe they never keep 1 TB of data at one place..
    I just told you an Idea which comes within timeline of reading your comment and writing my comment.. ehehe
    So there are numerous of Ideas to do that.. It's very important for researcher to think out of box.

     

    mudz