Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog What can you do with a GHz MCU?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kjachim
  • Date Created: 25 Mar 2021 7:36 PM Date Created
  • Views 1087 views
  • Likes 1 like
  • Comments 0 comments
  • pci
  • graphics
  • arm cortex-m4
  • mcuxpresso
  • mipi
  • i.mx rt1170 family
  • arm cortex-m7
  • can fd
  • usb audio
  • ghz mcu
  • crossover mcu
Related
Recommended

What can you do with a GHz MCU?

kjachim
kjachim
25 Mar 2021


image

Despite the thousands of development boards that have shipped and the overwhelming interest from the market for the i.MX RT1170 crossover MCU, I do come across an occasional customer that does not understand the value.  They say they do not need the performance or integration or security that the i.MX RT1170 MCU family offers.  More often than not though, they simply do not understand how these features could work for them in their applications.

 

Take, for example, applications in the IoT space, many are already reaping the benefits that come with combining the performance and unique feature set available with the i.MX RT1170 MCU family.   Smart home applications like thermostats and home appliances, are using the on-chip MIPI interfaces and graphics accelerators on the i.MX RT1170 to create more sophisticated UIs for consumers. Audio customers are using features like the HS USB for high-quality audio and taking advantage of the USB audio class enablement that is in NXP’s MCUXpresso Software and Tools for designing products like audio interfaces, mixers, and voice processors.  Point-of-sale applications leverage the PCI pre-certification with dedicated tamper pins, drone applications take advantage of CAN-FD for motor control, and smart signage applications also benefit from MIPI interfaces and graphic accelerators.

 

What do all of these applications have in common?  Regardless of the features set, they are also each taking advantage of the high performance to add new software features, improve response time, and/or run computationally-intensive algorithms quickly and efficiently.

 

The i.MX RT1170 actually includes 5 configurations, offering various levels of performance and integration, so that customers can choose the specific configuration that is best-suited for their particular application

 

image

 

 

Want to learn more?  Get started today by diving into latest i.MX RT1170 training content at
nxp.com/iMXRT1170/training