Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog XBOX XIM 3 teardown and analysis
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 14 Mar 2011 11:04 PM Date Created
  • Views 4322 views
  • Likes 0 likes
  • Comments 8 comments
  • research
  • xbox
  • microchip
  • xim
  • embedded
  • gaming
  • microcontroller
  • engineering
  • nxp
  • innovation
  • xim3
Related
Recommended

XBOX XIM 3 teardown and analysis

Catwell
Catwell
14 Mar 2011
image
 
The XIM 3 stand for XBOX Input Machine version 3. For those  who do not know, the XIM 3 allows for a keyboard, mouse, joystick, and other USB based devices to be adapted to the console. But that is not the end of the device's features. In many games a little autoaim functionality is added to help the player aim using a controller, since the controller is not the most precisely controlled input device. The XIM 3 has onboard software called "Smart Translators" that takes a particular game's aiming and movement actions and attempts to remove any autoaim and movement aids to give a PC like keyboard and mouse feel. Let's take a look at this achievement from the inside.


imageimage
 
The device is stylish and does not feel cheap. The casing, a dense plastic, sits the screen at an angle allowing the player to see the information while seated as if at a desk, within the LCD's viewing angle. 3 A type USB ports are on the back for, presumably, a keyboard, mouse, and XBOX controller. The XBOX controller is needed, ultimately, for sending the control signals to the console. The XBOX addresses a controller and expect signals. The XIM piggybacks on the controller signal. A mini usb port is present for a connection to the XBOX console itself. A barrel plug for a power adapter is also present, which may be needed at a user adds a USB hub for more devices.


image
 
The XIM 3 shell is held together with 2 visible screws and two underneath foot-pads. Inside shows the screen ribbon cable connected to the mainboard on the base. The screen model number is SG100331. Ribbon cable is marked TS8001S FKJ40010 V1.0. The LCD is a QVGA panel


imageimage
 
The mainboard has a model name HDDC3C02 made by HDDC inc. No information could be found on the company or model number. However, the central microcontoller is a NXP - LPC1768FBD100LPC1768FBD100. A cortex M3 100Mhz 32 Bit ARM processor with 65KB RAM and 512KB program memory space. On the mainboard is a Texas Instruments TUSB2046BTUSB2046B 4-port Full-Speed USB Hub, hence XIM3's 4 ports. (The hub requires 3.3V, the assumption is that the NXP ARM is also run at the same voltage.) Also present is a MAX3421EE USB peripheral host controller with SPI interface. This controller digital logic and analog circuitry necessary to implement a full-speed USB peripheral, or in this case the T.I host controller. (Supply voltage for the MAX chip is also 3.3V) Not to surprise anyone, but a LD33 F022 (3.3V) linear voltage regulator powers the whole system. My only complaint about the system are the experience I had with the 3 main USB ports. It was easy to bend a pin out of place, impeding cable inserts. However, I bent the pins back in place, and all was well.


image
 
 
There is no additional memory, so the entire program sits in 512KB. Overall, it is an impressive design, circuit, packaging, and the code must be exquisite. This is an example of only one person accomplishing an amazing feat on his own. Inspiration to all of us and our ideas.

 
XIM 3 units are finally available at the XIM Technologies website on a regular basis. When the XIM was first released, the attention and web traffic was so great that it crashed the servers. After the website's servers were upgraded, "OBsIV" the creator of XIM, would only open the store privately for short periods, like 5 minutes. The only way to the store was knowing the direct address, and was not available from the home page. Some people were using other services, like "alertbox," to monitor when the site would open. Eventually, everyone who desperately wanted one, now has one. For the record, the one pictured above was purchased in a 5 minute window in February.

 
Want to know how the device performs in games? I will relate my experiences in an up and coming post.

 
Cabe
  • Sign in to reply
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    I would newer buy that device and cannot understand people who would do. When I play on console I enjoy pad, if I want to play using mouse I use PC. Simple as that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Eavesdropper
    Eavesdropper over 15 years ago in reply to e14 Contributor

    It is like using a gamepad to navigate the Window operating system vs. using a mouse. You can get used to both, but one will give you more precise control.

     

    All the precision is in your thumb or in your arm and wrist. Again, one is more accurate, but that is based on preference.

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Eavesdropper

    I think that one of the reasons that XBOX do not support mouse is fact that mouse users have more precision indeed so it would be unfair to let them compete with pad users. That's why there are no mixed PC-console matches, in my opinion using such device is just cheating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Eavesdropper

    I think that one of the reasons that XBOX do not support mouse is fact that mouse users have more precision indeed so it would be unfair to let them compete with pad users. That's why there are no mixed PC-console matches, in my opinion using such device is just cheating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Catwell
    Catwell over 15 years ago in reply to e14 Contributor

    Since I did this tear down I have used the mouse extensively in all my games.

     

    For the most part, I have brought my gaming level up. I am usually towards the top of the score board. However, people still get the drop on me.

     

    I would not call this cheating. It is just an alternative controller.

    However, if you are in competition (which most of us are not) I am sure they may raise an eyebrow to the mouse setup.

     

     

    The firmware has been updated, making the over all operation smoother.

     

    Cabe