Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Analogue Design 9V NiMH charging
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 526 subscribers
  • Views 4011 views
  • Users 0 members are here
  • charging
  • nimh
  • battery
Related

9V NiMH charging

koudelad
koudelad over 2 years ago

Hello,

9V batteries have always been a pain for me... Expensive, low capacity, almost every DMM / tester needed them.

I just bought a 9V NiMH battery: https://www.westinghousebattery.com/Ni-MH-Rechargeable/Premium-Series.html . To my surprise, it is not made from 6 smaller cells (which would give ca. 7.2-8.4 V), but 7, which has nominal voltage of 8.4, but when charged, can have almost 10 V. This makes it a true primary 9V battery replacement. I am not sure when these became available, but I remember older 6-cell "9 V" NiMH that were kind of useless, because all appliances thought the battery is discharged, due to the lower nominal voltage.

However, I never really had a charger for this kind of battery. I have heard that cheap chargers only use 12 V DC power supply with in series resistor in series to limit the current to ca 30 mA.

Do you have any suggestion for a charging circuit? I am open to building something, even using an MCU. I would love it to have a small small charging current (20-30 mA) or slightly higher (50 mA), a safety timer and the delta V detection. There is a famous old MAX713 charger, but according to the features, it offers C/4 to 4C charging and C/16 trickle charging, which is too high. Most commercially available hobby chargers also have a minimum current of 100 mA.

Thank you,

David

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago in reply to shabaz +5
    I had some time, to lay out the PCB. This board is 100 x 60 mm and several different PP3 battery holders will fit. All parts are jellybean. The optional microcontroller is connected to the row of pin-headers…
  • shabaz
    shabaz over 2 years ago +3
    I think the circuit below would do it. It's based off of a simpler charger here: Smart Doorbell System – Part 6 – Chime Module Complete Circuit Design and based on information from a battery mnfr PDF doc…
  • genebren
    genebren over 2 years ago in reply to shabaz +3
    Very Nice! This is something that I would like to look into further in the future. I really do appreciate your efforts to assist and to promote a true sense of community here on element14!
  • shabaz
    0 shabaz over 2 years ago in reply to shabaz

    It was bugging me that there wasn't a timeout. I've been in the position where I've forgotten to unplug a charger.

    The timer needs to be somewhere in the region of 16-24 hours. The design below (untested) uses a load of divider chips. It looks a lot, but 74HC4060 are cheap (and probably there's no size restriction). All parts here shouldn't cost more than a few $ total.

    The crystal output is just divided loads, and when 19 hours is reached, the TIMER_EXPIRY signal goes high, and that also prevents any more counting.

    image

    The timer isn't essential, and if there's a microcontroller attached, then it's redundant (unless such a hardware timer is preferred).

    The main circuit is tweaked to add the TIMER_EXPIRY connection as an input:

    image

    Also, while I was at it, I replaced the constant current resistor with a rotary selector, since it appears there are PP3 batteries with a range of capacity. Probably overkill to have such granularity, but the rotary switch could be replaced with a wire link to permanently set a current if desired.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • koudelad
    0 koudelad over 2 years ago in reply to shabaz

    Thank you, but to be honest, I think a single 8-bit 6-pin MCU would replace the timing circuit and maybe also the charging logic.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to koudelad

    Yes, it would be greatly simplified with a microcontroller.

    I'll document the rest somewhere and maybe finish it if it helps anyone.

    I couldn't settle on a target microcontroller (and didn't fancy coding anything currently), so I figured I may as well make it microcontroller-agnostic, i.e., one could unpopulate those additions if the microcontroller interface is used.

    It's just a mental exercise, I have no serious suggestion for anyone to construct this unless they enjoy soldering a lot of parts. Plus, my design decisions won't be the same as others; I just used what parts I was familiar with (I'd already tested that constant-current portion in that Bluetooth project, so I lifted that as-is).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ariajames_121
    0 ariajames_121 over 1 year ago

    It’s great that you found a true 9V replacement with 7-cell NiMH batteries since older 6-cell versions always had voltage issues. For charging, a proper circuit with delta-V detection and a safety timer would be ideal. You could consider designing a custom circuit using an MCU with a constant current source and termination detection. If you want a simpler approach, a low-current linear regulator with a series resistor can work, but it may not be as efficient or safe in the long run. Have you looked into smart chargers like the La Crosse or Opus models?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<