Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
DSP Forum Circuit Diagram is needed for the following features
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 167 subscribers
  • Views 520 views
  • Users 0 members are here
Related

Circuit Diagram is needed for the following features

e14 Contributor
e14 Contributor over 13 years ago

I have to design a crcuit which will have following features:

 

        I/P: X15 X14 X13... ... ...X0 bits

        O/P: 1, when I/P bit sequence has 3 consecutive ones

           or atleast 3 consecutive ones.

 

Would u pls show me the circuit diagaram needed for this requirement?

 

thanx in advance

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Can't be much simpler: 14 three-input NANDs, each connected to three successive input bits:

    X15, X14, X13 => NAND13;

    X14, X13, X12 => NAND12;

    .

    .

    .

    X2, X1, X0 => NAND0;

     

    Then the 14 outputs get NANDed together via a 14 input NAND.

     

    Output goes high if and only if three or more successive bits are high.

     

    All of which should fit nicely in any tiny CPLD, PAL, etc. A one-chip fast, unclocked solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Can't be much simpler: 14 three-input NANDs, each connected to three successive input bits:

    X15, X14, X13 => NAND13;

    X14, X13, X12 => NAND12;

    .

    .

    .

    X2, X1, X0 => NAND0;

     

    Then the 14 outputs get NANDed together via a 14 input NAND.

     

    Output goes high if and only if three or more successive bits are high.

     

    All of which should fit nicely in any tiny CPLD, PAL, etc. A one-chip fast, unclocked solution.