Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
DSP Forum Algo for rms computation?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 166 subscribers
  • Views 3111 views
  • Users 0 members are here
Related

Algo for rms computation?

ggabe
ggabe over 3 years ago

I’m entertaining a true rms computation on MSPM0G3507 for the 10Hz…100KHz range. 

The MCU is limited to 32K RAM, so I’d change the sampling frequency if I can determine the signal is periodic and in the lower frequency range.

Is there any algorithm that aims capture N periods of a periodic signal? 

Should I be better of by going into frequency domain with a proper window function, and possibly trying multiple sampling rates to choose the proper range?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +1
    What's wrong with: sample (at 500kHz) s square (at 500kHz) sq = s * s mean (at 500kHz) m = m + ( (sq - m) / Ki) square root (at read out rate) rms = m ^ 0.5 Division by a constant can be done…
  • ggabe
    ggabe over 3 years ago in reply to scottiebabe +1
    Yes, it is interesting. TI is selling the EVB for $16 direct. The part is very much a new item, TI is not sampling it yet. The accelerator is cool, but not as advanced as the MSP430's LEA. The benefit…
  • ggabe
    ggabe over 3 years ago in reply to michaelkellett +1
    I think the algorithm with Ki used to be referred as exponential decay averaging. The alternative, the moving averaging has a sensitivity when the weight of the partial periods start to influence the average…
Parents
  • scottiebabe
    scottiebabe over 3 years ago

    Interesting chip!

    image

    I didn't see the cycle counts for the math co-processor but it looks interesting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ggabe
    ggabe over 3 years ago in reply to scottiebabe

    Yes, it is interesting. TI is selling the EVB for $16 direct. The part is very much a new item, TI is not sampling it yet. The accelerator is cool, but not as advanced as the MSP430's LEA. 
    The benefit for me is no need for noisy SPI bus between ADC and CPU, and I can treat the MCU, once programmed, as a single part RMS converter.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ggabe
    ggabe over 3 years ago in reply to scottiebabe

    Yes, it is interesting. TI is selling the EVB for $16 direct. The part is very much a new item, TI is not sampling it yet. The accelerator is cool, but not as advanced as the MSP430's LEA. 
    The benefit for me is no need for noisy SPI bus between ADC and CPU, and I can treat the MCU, once programmed, as a single part RMS converter.