Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Seeking the 5 Most Interesting, Amazing or Exciting Industrial Single Board Computer Applications
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 508 subscribers
  • Views 2049 views
  • Users 0 members are here
  • industrial sbc aplications
  • Single Board Computer
  • exciting applications
Related

Seeking the 5 Most Interesting, Amazing or Exciting Industrial Single Board Computer Applications

rscasny
rscasny over 6 years ago

Single Board computers (SBC) are amazing little devices in their own right. They pack a lot of technology in an incredibly small footprint. They are used for all kinds of projects by students, hobbyists and professionals. They have been used gaming, telecom, and other automation applications. They are also used to inspire and teach programming in schools. Over the last few years, I have seen more and more attention paid to using SBCs in industrial applications. I've learned "industrial" in this context means different things to different people. Sometimes it just means a commercial product (e.g., media player, vending machine). I define industrial in a truer sense of the world: in a factory, in a machine, or in the field for control of actuators, etc.

 

I'm looking to get 5 interesting industrial applications of SBCs. Do you have any in mind? If you do, leave a comment and tell me more.

 

Thanks.

 

Randall

--element14 team

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 6 years ago +10
    The standard, not hardened SBCs can be the backbone for instrument automation. The hardened ones can be the core for small size shop floor data collection / MES systems, and edge devices for exchange with…
  • ntewinkel
    ntewinkel over 6 years ago +9
    Didn't they use a Raspberry Pi for something at the large hadron collider? I wasn't able to find that, but while searching found this pretty cool project by CERN, using Raspberry Pis: https://www.raspberrypi…
  • 14rhb
    14rhb over 6 years ago +8
    The main one that springs to mind for me is this. Many of the homemade 3D printers use an Arduino Mega 2560 SBC and an accessory board called RAMPS, and more specifically people are using that low-cost…
Parents
  • dougw
    dougw over 6 years ago

    What is your definition of a single board computer?

    To me an SBC is a complete computer on one board - with processor, memory and user interface.

    The user interface is the gray area - does it need an HDMI port and a USB host port or is it enough to have a serial port for an external terminal?

    The first SBCs had a keypad and display right on the board - that is very rare these days.

    My first SBC (AIM65) had a full keyboard, alphanumeric display and printer right on the board.

    The SBC application that made the biggest splash here is probably PIK3A. The concept was good enough to be commerialized as PiCade.

    However, it isn't an industrial application.

    The only industrial application we use sometimes at work is an arduino that was part of a project where we sponsored some mechatronics students at a local college to design and build a pneumatic machine to run products through mechanical cycles for accelerated life testing. It doesn't have much of a user interface and the display is mainly just a cycle count, but it might qualify as an SBC by some definitions.

    I think the Beaglebone Blue is one of the top candidates for industrial SBC platforms, although I haven't seen it in anything beyond robots and drones yet.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 6 years ago

    What is your definition of a single board computer?

    To me an SBC is a complete computer on one board - with processor, memory and user interface.

    The user interface is the gray area - does it need an HDMI port and a USB host port or is it enough to have a serial port for an external terminal?

    The first SBCs had a keypad and display right on the board - that is very rare these days.

    My first SBC (AIM65) had a full keyboard, alphanumeric display and printer right on the board.

    The SBC application that made the biggest splash here is probably PIK3A. The concept was good enough to be commerialized as PiCade.

    However, it isn't an industrial application.

    The only industrial application we use sometimes at work is an arduino that was part of a project where we sponsored some mechatronics students at a local college to design and build a pneumatic machine to run products through mechanical cycles for accelerated life testing. It doesn't have much of a user interface and the display is mainly just a cycle count, but it might qualify as an SBC by some definitions.

    I think the Beaglebone Blue is one of the top candidates for industrial SBC platforms, although I haven't seen it in anything beyond robots and drones yet.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 6 years ago in reply to dougw

    I'm happy with your basic definition of an SBC, display optional - a control port will do.

     

    I think the reason that the popular and well known ones don't find many serious industrial applications is that in order to become popular they must be cheap and cover a wide range of applications. This means that they usually skimp on industrial features like long term availability and good real world robustness.

    For example, in industrial applications connectors are a major source of reliability issues and it is very unusual to pick the cheapest with enough pins and an adequate current rating, but to make a cheap SBC this is almost exactly what you do.

    The other issue is that the feature set on an SBC will rarely be a perfect fit, and while you can often stand having some unused hardware, all too often you end up needing an additional board.

    The RPI compute board looks like a reasonable attempt to get round some of these issues but I'm not at all sure how successful it has been.

     

    My use of ready made SBCs is limited to simple test jigs and fixtures, very few have ever made it out into a customer's hands, and those few have been as test or programming aids, not in saleable products.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down