Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Seeking the 5 Most Interesting, Amazing or Exciting Industrial Single Board Computer Applications
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 508 subscribers
  • Views 2021 views
  • Users 0 members are here
  • industrial sbc aplications
  • Single Board Computer
  • exciting applications
Related

Seeking the 5 Most Interesting, Amazing or Exciting Industrial Single Board Computer Applications

rscasny
rscasny over 6 years ago

Single Board computers (SBC) are amazing little devices in their own right. They pack a lot of technology in an incredibly small footprint. They are used for all kinds of projects by students, hobbyists and professionals. They have been used gaming, telecom, and other automation applications. They are also used to inspire and teach programming in schools. Over the last few years, I have seen more and more attention paid to using SBCs in industrial applications. I've learned "industrial" in this context means different things to different people. Sometimes it just means a commercial product (e.g., media player, vending machine). I define industrial in a truer sense of the world: in a factory, in a machine, or in the field for control of actuators, etc.

 

I'm looking to get 5 interesting industrial applications of SBCs. Do you have any in mind? If you do, leave a comment and tell me more.

 

Thanks.

 

Randall

--element14 team

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 6 years ago +10
    The standard, not hardened SBCs can be the backbone for instrument automation. The hardened ones can be the core for small size shop floor data collection / MES systems, and edge devices for exchange with…
  • ntewinkel
    ntewinkel over 6 years ago +9
    Didn't they use a Raspberry Pi for something at the large hadron collider? I wasn't able to find that, but while searching found this pretty cool project by CERN, using Raspberry Pis: https://www.raspberrypi…
  • 14rhb
    14rhb over 6 years ago +8
    The main one that springs to mind for me is this. Many of the homemade 3D printers use an Arduino Mega 2560 SBC and an accessory board called RAMPS, and more specifically people are using that low-cost…
Parents
  • gustavovelascoh
    gustavovelascoh over 6 years ago

    We used a RPi compute module for a central unit of an Access Control System. We developed a custom host board for it and it has different versions.

    Actuators are controlled using a microcontroller, which also is connected to an RFID reader. The microcontroller uses SPI to talk to the RPi. The RPi communicates to the server using a Giga Ethernet port for sending reports and downloading permissions data. There are versions with Servomotors and EM locks as actuators, both using direct control or through RS485.

    In a newest version, 2 main features were added to the RPi section of the device: Support for two cameras (CSI) and Bluetooth via serial using a nRF52. The application is a movement detection Bluetooth network which triggers the capturing of pictures, and from the existing access control events, recording is started as well.

     

    Several devices from the earlier version have been running for 5-6 years now and for the newer version, it could be something around 3 or 4 years.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gustavovelascoh
    gustavovelascoh over 6 years ago

    We used a RPi compute module for a central unit of an Access Control System. We developed a custom host board for it and it has different versions.

    Actuators are controlled using a microcontroller, which also is connected to an RFID reader. The microcontroller uses SPI to talk to the RPi. The RPi communicates to the server using a Giga Ethernet port for sending reports and downloading permissions data. There are versions with Servomotors and EM locks as actuators, both using direct control or through RS485.

    In a newest version, 2 main features were added to the RPi section of the device: Support for two cameras (CSI) and Bluetooth via serial using a nRF52. The application is a movement detection Bluetooth network which triggers the capturing of pictures, and from the existing access control events, recording is started as well.

     

    Several devices from the earlier version have been running for 5-6 years now and for the newer version, it could be something around 3 or 4 years.