Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum How to convert PID output into meaningful result to feed into controller
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 503 subscribers
  • Views 1465 views
  • Users 0 members are here
  • pid controller
Related

How to convert PID output into meaningful result to feed into controller

chrischristian14
chrischristian14 over 6 years ago

Hi, I am creating a pressure controller with PIC micro that is controlling the heating coil and a pocketbeagle that is running a PID loop. The PIC micro takes commands from pocketbeagle over UART.

PIC responds to 0 to 9, with 9 being heating coil switched off and 1 being full on.The PID loop outputs numbers up to 10000000, depending upon what is the difference between the measured pressure and the desired pressure, and I am really struggling to convert this PID output (0 to 10 million ) to a range of 0 to 9 and not killing the PID functionality - i.e. keeping it PID and not making it like a normal code. I managed to have a few range of loop, and each range is a PID loop on its own, but that is not an ideal solution. Below is the code I tried, int_diff is the (int) PID output. Can anyone pelase help ? I have a feeling I might be over complicating things but don't know how.

Just to explain, in below code, each range sends 0 to 9 numbers to PIC micro, so the problem arises when the difference between set pressure and measured pressure is low and it just need to go up by a little, but the output (int_diff) switches range and suddenly it goes to 0 (heating coil full on) and then on next measurement (after about a second) it goes to 9 (heating coil off), while it should be moving from 8 to 9. This kind of movement (0 to 9) causes overshoot, and the reverse is also true, causing very slow rise in temperature or undershoot.

I hope I am making sense. Thanks

if(0<int_diff && int_diff<99)
{
value = diff/10; //(gives 1 to 9)
closer =1;
}
#if 1
else if(99<int_diff && int_diff<999)
{


value = diff/100;
closer =1;
}




else if (999<int_diff && int_diff<9999)
{
value = diff/1000;
closer =1;
}
else if (9999<int_diff && int_diff<99999)
{
value = diff/10000;
closer =1;
}




else if (99999<int_diff && int_diff<999999)
{
value = diff/100000;
closer =1; 
}
else if (999999<int_diff && int_diff<9999999)
{
value = diff/1000000;
closer =1;
//value = 0;
}




if(closer==1)
{


if(value>=0)
{
value= 9-(int)value;
}
else if(value<0)
{
value=9;
}


}
else
{
value = 0;
}

  • Sign in to reply
  • Cancel

Top Replies

  • chrischristian14
    chrischristian14 over 6 years ago in reply to michaelkellett +3
    Thanks Michael, I am not new to this embedded stuff, I have about 10 years of experience in electronics and maintain an RTOS product as part of my full time work, what I am not good at is explaining things…
  • michaelkellett
    michaelkellett over 6 years ago +2
    Not making much sense ! This doesn't look like all your code ! You would do much better to have it all in one place either on the PIC or the Beagle. Steps of only 0 to 9 is quite possibly not fine enough…
  • michaelkellett
    michaelkellett over 6 years ago in reply to chrischristian14 +2
    I get the feeling you are new to all this embedded stuff. My first bit of advice is that you should never leave an unexplained observation to fester. You say that the triac turns on and then turns off…
Parents
  • genebren
    genebren over 6 years ago

    Chris,

     

    This is a little complex, but not in a good way.  Unless you need the PIC for other things, why not drive the heating coil switch directly from the pocketbeagle?  If the PIC has some other useful function, and you need to drive the heating coil switch from it, why not skip the UART ans communicate the PID output via something like a PWM signal (having a much greater range than 10 discrete levels).  The PIC could read the PWM signal as an analog input (passed through a low pass filter to convert the PWM to a DC signal).  This could allow the PID loop to be a bit more continuous and eliminate the need for the limited range of control.

     

    Best of luck!

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 6 years ago

    Chris,

     

    This is a little complex, but not in a good way.  Unless you need the PIC for other things, why not drive the heating coil switch directly from the pocketbeagle?  If the PIC has some other useful function, and you need to drive the heating coil switch from it, why not skip the UART ans communicate the PID output via something like a PWM signal (having a much greater range than 10 discrete levels).  The PIC could read the PWM signal as an analog input (passed through a low pass filter to convert the PWM to a DC signal).  This could allow the PID loop to be a bit more continuous and eliminate the need for the limited range of control.

     

    Best of luck!

    Gene