Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Writing protocols for bare-metal C
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 503 subscribers
  • Views 4335 views
  • Users 0 members are here
  • firmware
  • ip_iot
  • embedded
Related

Writing protocols for bare-metal C

ipv1
ipv1 over 6 years ago

Over the years, I come across the need to connect sub systems together with the like of UART, I2C, CAN, LIN, RS485, MODBUS and what not. A few years ago, I also wrote about implementing custom protocols that are simple versions of the previously stated ones and recently jumped into a project that uses a custom LIN implementation. By custom, I means that it does not follow the rules or LIN in terms of communication but uses the same electrical base and some other pieces.

 

The existing code base is heavily reliant on the processor registers etc and the guy who wrote it can't/won't explain the structure of the system as a lot of it is unplanned, undocumented patches. It works but its a lot of C code mixed with "other things".

 

My question here is about a standard way of writing things like these. I am talking about implementing multi-byte exchange protocols and what should be the do's don't, correct way, though processes, etc when writing this stuff. Finite state machine code with non-blocking code is where I usually land but I want your thoughts on the process.

 

What is your way of writing protocols without an OS and how would you accomplish multiple tasks with out the scheduler?

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Jan Cumps +5
    While I'm at it: never consult hardware/firmware forums when thinking about version control. They are inventing issues that have been solved in 1985 .... and say that firmware development is unique. And…
  • michaelkellett
    michaelkellett over 6 years ago in reply to ipv1 +5
    There's a lot to be said for the "Superloop plus interrupts" architecture - but like everything it has its place and gets used in the wrong places. For simple systems it has lots of advantages - not the…
  • shabaz
    shabaz over 6 years ago +4
    Hi Inderpreet, In telecoms there's lots of protocols documented, but there's no (publicly available) source code often, so it's up to the software developer to code it. The way the protocol is documented…
  • Jan Cumps
    Jan Cumps over 6 years ago

    I always use a standard protocol. Even if I don't like it or can see shortcomings.

     

    It helps myself and my colleagues in the long run.

    All in your list are fair game as a protocol I'd use. The decision would be based on topology (on-board- wired, long-distance wired, industrial,  ...)  and what's already used in a design.

     

    The same for OSes. I will always use an existing OS protocol  In RTOS, that's typically tasks, queues, messaging and metaphors.

    In Linux/Windows/... any of the existing protocols, from sockets up to MQTT, web services, RPCs, ..., domain specific APIs).

    Any protocol my colleagues or myself invented "because they were better" turned into an unsupported pile  of trash. One of the reasons why I'm sticking to SCPI (and love it).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • ipv1
    ipv1 over 6 years ago in reply to Jan Cumps

    I understand and agree. My problem starts with the fact that most hardware guys are not trained to thing in software. In many cases I don't really have a choice hence the question.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to ipv1

    ipv1  wrote:

     

    I understand and agree. My problem starts with the fact that most hardware guys are not trained to thing in software. In many cases I don't really have a choice hence the question.

    That's one of the arguments why I think that hardware guys should shy away from inventing "better" protocols.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Jan Cumps

    While I'm at it: never consult hardware/firmware forums when thinking about version control.

     

    They are inventing issues that have been solved in 1985 .... and say that firmware development is unique. And advice zip files. Copies. Dropbox. More copies, directories that have a version as their name...

    Then they make the errors peoples in 1984 made ...

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago

    Hi Inderpreet,

     

    In telecoms there's lots of protocols documented, but there's no (publicly available) source code often, so it's up to the software developer to code it. The way the protocol is documented can vary, but one method looks like flow charts, known as SDL.

    It can be used to describe pretty complex protocols. SDL allows you to describe message sequences, error states, timeouts, timers etc. So if a designer wished to design and document a protocol that would be one way, and it's accepted by telecoms software engineers, they can take it and run with it, and churn out a protocol stack in software.

     

    In a more rapid world, people would write an RFC* (Request for Comment).. it would be public and people would scrutinize it : ) pick holes in it and write updates.

     

    I think (for new situations) there's nothing wrong with lifting a protocol and inserting it into a different lower-layer, or tunneling a protocol in another, or using a protocol for a different or newer purpose, or (sometimes) adding extensions. All of these are very common in the networking world.

    Writing a totally custom protocol (even if it is on top of some well-known lower layers) while achievable, you have to ask, why would they do it.. sometimes it is to deliberately try to obscure. There was a time (about a decade ago) when company lawyers would frown on that, because interfaces were subject to the 'Software Directive'. It literally gave free permission to anyone to reverse-engineer your product, if they couldn't obtain a copy of the spec. That legislation is superseded now. Reverse-engineering was (to some, not to me!) undesirable because you always ran the risk that the person who was doing the reverse-engineering may discover more tips and tricks and proprietary stuff that go beyond what was required to understand the interfacing protocol..

     

    * Example.. this one documents information transfer with layer 1 being carrier pigeon : )

    https://tools.ietf.org/html/rfc1149

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz

    shabaz  wrote:

     

    Hi Inderpreet,

     

    In telecoms there's lots of protocols documented, but there's no (publicly available) source code often, so it's up to the software developer to code it. The way the protocol is documented can vary, but one method looks like flow charts, known as SDL.

    It can be used to describe pretty complex protocols. SDL allows you to describe message sequences, error states, timeouts, timers etc. So if a designer wished to design and document a protocol that would be one way, and it's accepted by telecoms software engineers, they can take it and run with it, and churn out a protocol stack in software.

     

    In a more rapid world, people would write an RFC (Request for Comment).. it would be public and people would scrutinize it : ) pick holes in it and write updates.

     

    I think (for new situations) there's nothing wrong with lifting a protocol and inserting it into a different lower-layer, or tunneling a protocol in another, or using a protocol for a different or newer purpose, or (sometimes) adding extensions. All of these are very common in the networking world.

    Writing a totally custom protocol (even if it is on top of some well-known lower layers) while achievable, you have to ask, why would they do it.. sometimes it is to deliberately try to obscure. There was a time (about a decade ago) when company lawyers would frown on that, because interfaces were subject to the 'Software Directive'. It literally gave free permission to anyone to reverse-engineer your product, if they couldn't obtain a copy of the spec. That legislation is superseded now. Reverse-engineering was (to some, not to me!) undesirable because you always ran the risk that the person who was doing the reverse-engineering may discover more tips and tricks and proprietary stuff that go beyond what was required to understand the interfacing protocol..

    If your design is worth the money you earn for it, it's going to be reverse engineered in the 2020s.

    I think that if you invented a new/better protocol, and no-one bothered to hack it - you wasted money and resources because no-one cares. And you have to maintain your legacy.

    A cost that you'll have to carry along forever without a competitive gain. Yes, you may tie some existing customers to your bespoke solution. But who wants to join your customer base?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to Jan Cumps

    I understand that.. but to some (again not me!) lawyers it was super-undesirable to legitimise it.

    The reason is, even if you don't have fancy tips/tricks/proprietary secrets, you run the risk that the person discovers _that_... and then uses it against you, by (say) finding the weaknesses and demonstrating them, and coming out with literature which then legally and rightly trash your product by pointing out these flaws.

    Using a standard protocol, and the problem went away from legitimate (operating within the law) competitors to some partial extent..

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz

    Have they ever measured the lawsuit costs versus developing-and-maintaining-proprietary costs?

    They have to sue people that steal their idea (secret or hidden behind closed source) in court - and that's expensive. Blaming and pointing doesn't do the job.

    That goes for ideas based on open and closed protocols. So the proprietary protocol may slow down competitors --- only if your idea isn't worth stealing ...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to Jan Cumps

    I'm saying the opposite..

    i.e. that the smart lawyers understood to use standards-based protocols. Using standards-based protocols bought you more time, because you've then eliminated the legitimately operating firms from being able to legally reverse-engineer to find out the interface.

    The law was that if you _didn't_ publish the interface (i.e. it was a proprietary interface) then you've given legitimate firms free permission to knock themselves out and go ahead with their software reverse-engineering, to create products to connect with yours... and in the process, run the risk they discover everything else, tips, tricks, skeletons, warts and all, about your product.

     

    Firms that didn't think that step, may well have not cared what their engineers used, and let them code proprietary stuff and usually that's silly - as I think you're saying too.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • ipv1
    ipv1 over 6 years ago

    All good points. I think the SDL thing is useful and I can see myself using that. Like you pointed out, there is rarely any implementation or code for protocols so any pointers to relevant info would be useful.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
>