Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Need Help with CC3000/ CC3100 Antenna design.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 502 subscribers
  • Views 1854 views
  • Users 0 members are here
  • cc3000
  • cc3100
Related

Need Help with CC3000/ CC3100 Antenna design.

gsgill112
gsgill112 over 6 years ago

Hi All,

I was going through my old stock of Modules and I found couple of CC300 MOD without embedded Ant.

 

I know How to use CAD apps like Eagle and KiCAD but have never designed any Antenna based Module ?

 

Can anyone help me with standard components as I don't have any means to buy any fresh Inductors/ Caps for a tuning circuits ??

 

Regards,

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 6 years ago in reply to gsgill112 +3
    Have a look this for PCB antennas . I haven’t used it but know someone who did.
  • jc2048
    jc2048 over 6 years ago in reply to gsgill112 +3
    These application notes contain designs for 2.4GHz pcb antennas https://www.ti.com/lit/an/swru120d/swru120d.pdf https://www.ti.com/lit/an/swra117d/swra117d.pdf
  • shabaz
    shabaz over 6 years ago +3
    Hi Gurinder, The CC3000 is best thrown away however, because it's very obsolete. It was not made by TI for very long, about 8 years ago. I'm guessing it had issues or was experimental. If you mean CC3100…
Parents
  • shabaz
    shabaz over 6 years ago

    Hi Gurinder,

     

    The CC3000 is best thrown away however, because it's very obsolete. It was not made by TI for very long, about 8 years ago.

    I'm guessing it had issues or was experimental.

    If you mean CC3100 then you'll find lots more information for that and it's a very mature stable product.

    Another option (if you don't wish to implement a PCB antenna) is to put an SMA connector on the board, and screw on an antenna.

    Here's an example, this is with CC3220 module.

    Not much to say about it, except that the track to the connector is about 0.8 mm thick, and the gap to the ground plane is 0.15 mm.

    The holes are 0.4 mm diameter, and separated about 1.6 mm. There's a ground plane on the other side too of course (1.6 mm thick PCB).

    You can use different values if required/desired, calculate the values from here. All the low-cost PCB manufacturers might not like 0.15 mm gap, but it's marginal and they may let you do it.

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz

    shabaz  wrote:

     

    Hi Gurinder,

     

    The CC3000 is best thrown away however, because it's very obsolete. It was not made by TI for very long, about 8 years ago.

    I'm guessing it had issues or was experimental.

    ...

    It's worth checking support for any CCxxxx device. Not only if it's advised for active production or not.

    Also if it is supported in recent RTOS and SDK releases.

    I have wifi, bluetooth and sub-1 GHz devices of that CC family and each of them has been abandoned in later software releases.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz

    shabaz  wrote:

     

    Hi Gurinder,

     

    The CC3000 is best thrown away however, because it's very obsolete. It was not made by TI for very long, about 8 years ago.

    I'm guessing it had issues or was experimental.

    ...

    It's worth checking support for any CCxxxx device. Not only if it's advised for active production or not.

    Also if it is supported in recent RTOS and SDK releases.

    I have wifi, bluetooth and sub-1 GHz devices of that CC family and each of them has been abandoned in later software releases.