Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Need Help with CC3000/ CC3100 Antenna design.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 502 subscribers
  • Views 1854 views
  • Users 0 members are here
  • cc3000
  • cc3100
Related

Need Help with CC3000/ CC3100 Antenna design.

gsgill112
gsgill112 over 6 years ago

Hi All,

I was going through my old stock of Modules and I found couple of CC300 MOD without embedded Ant.

 

I know How to use CAD apps like Eagle and KiCAD but have never designed any Antenna based Module ?

 

Can anyone help me with standard components as I don't have any means to buy any fresh Inductors/ Caps for a tuning circuits ??

 

Regards,

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 6 years ago in reply to gsgill112 +3
    Have a look this for PCB antennas . I haven’t used it but know someone who did.
  • jc2048
    jc2048 over 6 years ago in reply to gsgill112 +3
    These application notes contain designs for 2.4GHz pcb antennas https://www.ti.com/lit/an/swru120d/swru120d.pdf https://www.ti.com/lit/an/swra117d/swra117d.pdf
  • shabaz
    shabaz over 6 years ago +3
    Hi Gurinder, The CC3000 is best thrown away however, because it's very obsolete. It was not made by TI for very long, about 8 years ago. I'm guessing it had issues or was experimental. If you mean CC3100…
Parents
  • gsgill112
    gsgill112 over 6 years ago

    So, rechecked

    I have about 6 x C3000 MOD, 2x CC3100 MOD R and 4 x CC3200 MOD R , any reference designs for making it into a dev board anyone ?

     

    Regards,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to gsgill112

    Hi Gurinder,

     

    Was it definitely an antenna issue, or could it be something else? Were you able to get the LED blinking for example?

    Capacitors are needed on the supply rails for the WiFi to work, it has higher current demand.

    Also, you picked the worst option; the CC3000 may not work with recent WLAN configurations, if it doesn't support the latest ciphers.

    I don't know if it does or does not. I just know the CC3000 is obsolete for a long time.

    The CC3100 or CC3200 would have been the better option. The CC3100 is still in shipping products, so I believe it should work with modern WiFi routers.

    I'm guessing the same for the CC3200, but you can check the TI website for its status and check CCS as Jan mentions.

     

    For prototyping with these style modules, there's a different way, so you can more easily see if the connections are correct.

    If you get any proto board (say perf-board) then you can stick the CC3xxx module on it up-side down, and then use very short lengths of very thin wire (either enamelled copper wire, or, way better, Kynar or Tefzel wire of 30AWG size) to patch from the pads of the CC3xxx to the nearest hole on the perf-board. I've used that method with success with the CC3xxx series. To eliminate solder blobbyness, use 0.38mm solder _maximum_, ideally thinner. 0.5mm is too thick. You'll need an excellent pair of wire strippersexcellent pair of wire strippers and at least semi reasonable tweezerssemi reasonable tweezers to use the Kynar wire but it's worth it.

    If there is a center pad on the module, then that needs connecting to ground too. Also, all other grounds are to be connected together. And use surface-mount 100nF across the supply rails, as close as possible, and then a larger capacitor fairly nearby (a couple of centimeters distance max) too.

     

    Regarding antenna design, Frank and Jon have supplied the detail. For a test board, I used the SMA connector method as you did, and it was successful.

    Dumb question, but did you check that you really do have a mating SMA plug and socket? Some consumer antennas use reverse-SMA, and if you screw that to a normal (non-reverse-SMA) SMA connector, then the center connection is not made. That would definitely not work.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 6 years ago in reply to gsgill112

    Hi Gurinder,

     

    Was it definitely an antenna issue, or could it be something else? Were you able to get the LED blinking for example?

    Capacitors are needed on the supply rails for the WiFi to work, it has higher current demand.

    Also, you picked the worst option; the CC3000 may not work with recent WLAN configurations, if it doesn't support the latest ciphers.

    I don't know if it does or does not. I just know the CC3000 is obsolete for a long time.

    The CC3100 or CC3200 would have been the better option. The CC3100 is still in shipping products, so I believe it should work with modern WiFi routers.

    I'm guessing the same for the CC3200, but you can check the TI website for its status and check CCS as Jan mentions.

     

    For prototyping with these style modules, there's a different way, so you can more easily see if the connections are correct.

    If you get any proto board (say perf-board) then you can stick the CC3xxx module on it up-side down, and then use very short lengths of very thin wire (either enamelled copper wire, or, way better, Kynar or Tefzel wire of 30AWG size) to patch from the pads of the CC3xxx to the nearest hole on the perf-board. I've used that method with success with the CC3xxx series. To eliminate solder blobbyness, use 0.38mm solder _maximum_, ideally thinner. 0.5mm is too thick. You'll need an excellent pair of wire strippersexcellent pair of wire strippers and at least semi reasonable tweezerssemi reasonable tweezers to use the Kynar wire but it's worth it.

    If there is a center pad on the module, then that needs connecting to ground too. Also, all other grounds are to be connected together. And use surface-mount 100nF across the supply rails, as close as possible, and then a larger capacitor fairly nearby (a couple of centimeters distance max) too.

     

    Regarding antenna design, Frank and Jon have supplied the detail. For a test board, I used the SMA connector method as you did, and it was successful.

    Dumb question, but did you check that you really do have a mating SMA plug and socket? Some consumer antennas use reverse-SMA, and if you screw that to a normal (non-reverse-SMA) SMA connector, then the center connection is not made. That would definitely not work.