Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Old OScope - Worth 100$?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 502 subscribers
  • Views 1080 views
  • Users 0 members are here
  • vintage
  • cro
  • oscilloscope
Related

Old OScope - Worth 100$?

navadeepganeshu
navadeepganeshu over 5 years ago

I have an option to get this scope for 100$! Worth it? I am a newbie and help me make a decision.

My Usage: Student and Hobby Projects, Basic T&M.

 

APLAB 5 IN 1 TESTLAB 3744

 

Features:

  • Comprises of Several Instruments in One Package Dual Trace Oscilloscope, Component Tester/Comparator, Triple Output DC Power Source, Frequency Counter and Function Generator.
  • Oscilloscope with dc to 30MHz Bandwidth and 1 mv/div Sensitivity on Both Channels.
  • 140mm Rectangular CRT and 8 x 10 cm.
  • Display with Internal Graticule. 40ns/div to 0.2s/div Time Base.
  • Z Modulation (TTL Level). X-Y Operation.
  • TV Triggering Frame (V) & Line (H). LINE Trigger.
  • Component Tester / Comparator for Quick Evaluation of Component Characteristics.
  • Triple Output DC Source for External Use.
  • 100MHz Frequency Counter Measures Frequency of Function Generator or Waveform Displayed on Oscilloscope, Also from external Input or source.
  • Function Generator Operates in the Range of 0.02Hz to 2MHz with 50 ohms Output Impedance and Attenuation upto 60dB.

 

Product datasheet is attached hereby.

Attachments:
image3744 - 5 in 1 Testlab.pdf
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 5 years ago +4
    Hi Navadeep, I think you'd have fun with it, I used my first CRT-based 'scope a lot too. However, I cannot see from the document, but I think it is not a storage 'scope. This will make it hard to use for…
  • navadeepganeshu
    navadeepganeshu over 5 years ago in reply to shabaz +2
    Lit. Thanks shabaz for your advice. It totally makes sense that a scope without storage capability is pretty useless. The Picoscope looks great compared to any of the scopes in that price range(also 2204A…
Parents
  • shabaz
    shabaz over 5 years ago

    Hi Navadeep,

     

    I think you'd have fun with it, I used my first CRT-based 'scope a lot too.

    However, I cannot see from the document, but I think it is not a storage 'scope. This will make it hard to use for many experiments with (say) digital technology or microcontrollers. My first CRT scope was a storage one, and I used that capability a lot. So personally I would not get this APLAB 'scope.

    Another option (similar cost) is Picoscope 2000 series. I have the model 2205A, it is still quite basic, but it can store traces, so it's useful for looking at digital signals like I2C, UART and so on, as well as analogue signals. It has a signal generator too. As an idea, you could enter some Project14 competitions, and if you win, spend your prize on such a 'scope.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • navadeepganeshu
    navadeepganeshu over 5 years ago in reply to shabaz

    Lit. Thanks shabaz for your advice. It totally makes sense that a scope without storage capability is pretty useless.

     

    The Picoscope looks great compared to any of the scopes in that price range(also 2204A-D2). Thanks and I am looking forward for it somehow image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • navadeepganeshu
    navadeepganeshu over 5 years ago in reply to shabaz

    Lit. Thanks shabaz for your advice. It totally makes sense that a scope without storage capability is pretty useless.

     

    The Picoscope looks great compared to any of the scopes in that price range(also 2204A-D2). Thanks and I am looking forward for it somehow image