I don't know what kind of liquid, that you need to measure. But my sugestion is as follows
The description you are giving is a bit unclear, so are more precise answer is hard to give.
I would like to know the following
To elaborate on the problem:
- Min/Max size of the container : 1m Diameter 1m Tall / 10m Diameter 10m Tall (To make it easy, I am making it a cylinder)
- Type of liquid : Any & Possibly pressurized gas (propane, co2, etc)
- Container material : Steel
- Liquid Level changes : Once a day
- Weight is not measurable.
I believe this is solvable since liquid flow rate in a pipe is measurable from the outside, why not liquid level.
I like the idea of measuring capacitance!
Cabe
Well capacitance won't work with a steel container!
One plausible way to get ultrasound to work would probably be to mount a transducer on the bottom of the tank, and see if you can detect the reflection off the surface of the liquid. The air to steel acoustic impedance mismatch would probably rule out a top mounted system.
Another would be mount the transducer on a track along the side of the tank, then you'd run the transducer up and down the tank. I would venture you'd see a measurable increase in reflection amplitude as it moved from liquid to no liquid. The solution would be very ecxpensive though, not only would you need moving parts, but you'd need to use special goo between the transducer and the wall of the tank to ensure no air gaps.
Well capacitance won't work with a steel container!
One plausible way to get ultrasound to work would probably be to mount a transducer on the bottom of the tank, and see if you can detect the reflection off the surface of the liquid. The air to steel acoustic impedance mismatch would probably rule out a top mounted system.
Another would be mount the transducer on a track along the side of the tank, then you'd run the transducer up and down the tank. I would venture you'd see a measurable increase in reflection amplitude as it moved from liquid to no liquid. The solution would be very ecxpensive though, not only would you need moving parts, but you'd need to use special goo between the transducer and the wall of the tank to ensure no air gaps.