Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Design Challenge : The Amateur Fireworks Show
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 503 subscribers
  • Views 1085 views
  • Users 0 members are here
  • 32bit
  • 8_bit
  • 32_bit
  • 16_bit
  • microprocessor
  • microcontrollers
  • embedded
  • development
  • microcontroller
  • programmable_logic
Related

Design Challenge : The Amateur Fireworks Show

Catwell
Catwell over 16 years ago
Independence Day is coming up in the USA, and everyone likes to set off fireworks. But that usually consists of someone lighting the firework and running away like their life depended on it. And often enough, what is set off is quite anti climatic. So, my idea is to set off a series of plain, often boring, bottle rockets in a dramatic way, and not just one at a time. And the best part is, you can get 500 rockets for about $10 in some states.

-We need a way to electrically light each individual rocket, and be able to control in what order, and frequency each one is lit.

-To house the rockets, let's just house them in a bundle of tubes, each would have their own.
 
Let's, as a community, help make an exceptionally more fun, and way safer celebration.

I can't wait to see what we come up with.

Cabe
  • Sign in to reply
  • Cancel
Parents
  • WestfW
    WestfW over 16 years ago

    I saw/heard drum riffs being played on salutes (large firecrackers) as a demonstration of some comany's electronic firing system once.  They finished with an encore of "Shave and a haircut."  It was very impressive.

     

    A problem is that while bottle rockets are cheap, most electrical ignitors run about $0.50 each...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to WestfW

    There is probably a better way, but just a thought...  Regarding the electronic ignitors being $0.50each (and only one-time usage!!), how about buying a spool of Nichrome wire?  After cutting into very small sections and crimping the small Nichrome section in the middle of two lengths of "regular wire", it seems that you would have a very low-cost (possibly re-usable) fuse lighter.  It is fairly easy to get the Nichrome wire to be "red hot" on command with a little bit of ohms law design work.

     

    Respectfully,

    Steve  French
    President, Volt  Vision
    www.voltvision.com
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Catwell
    Catwell over 16 years ago in reply to e14 Contributor

    Interesting, the hurdle of lighting each fuse is the real challenge. 

     

    I was considering a spark plug like, arcing elements. Like how the cordless soldering irons work.

     

     

    Something else to consider, how can you control say 100 rockets? How can just one in particular be triggered? Multiplexing like a LED display might be the best option.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • enrico.migchels
    enrico.migchels over 16 years ago in reply to Catwell

    Hi,

     

    I like the idea of the Nichrome wire. I used bycicle headlights (6V/50mA) in the past to set of my explosions. You just crack the glass and insert the rockets ignition cord. It is also a 'one shot' option. If you use a traditional Christmas tree light you have lots of igniters. Bye the way, using words as 'igniters' and 'explosions' in our discussions; could this result in an investigation by some government agency? :-)

     

    Lot's of success (or good luck)

     

    Best regards, Enrico Migchels

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Catwell
    Catwell over 16 years ago in reply to enrico.migchels

    Enrico,

     

    I was thinking the same thing.

     

     

    But, I have a suggestion that could replace the Nichrome wire. Using small springs tied at either end by larger gauge wire. Then the spring almost acts like a light bulb filament.

     

    But more importantly, I want to know how to control a large matrix of transistors with only a few Gen IO pins from a uC. Ex: 100 transistors and 10 IO pins, for example. Any thoughts?

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • firatkocak
    firatkocak over 16 years ago in reply to Catwell

    Hi Cabe,

     

    You can control as many as transistors just 3 Mcu IO's using 74HC595 shift registers or equalevant chips having same function. If you give me more details about your design, i can make the schematics for you.

     

    If you decide to use 74HC595 then you need 13 chips. According to the use of the transistors ( sink or source ) and the power requirements you may need extra components.

     

    Firat

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to Catwell

    Cabe,

     

    Igniting your rockets this way will result in more or less severe timing differences.

     

    You can consider to group your rockets, say 5 or 10 per ignition instant. The group of rockets will go off with a nice whooooshhh (I imagine).

     

    Success !!!

     

    Klaus

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jason721
    jason721 over 16 years ago in reply to Catwell

    I was looking at building a Christmas display at one point controlled by a computer. You know the displays that go with the music. Something like that might work for you as well.Ths is set up for 120VAC because it was meant for lights but I know I saw an LED board set up as a working model of one of these circuits some where.

     

    Here is a link that I came accross if you look around there site they have a program on there to.

     

    http://discolitez.com/pmwiki/pmwiki.php?n=hardware.deluxe32

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jason721
    jason721 over 16 years ago in reply to Catwell

    I was looking at building a Christmas display at one point controlled by a computer. You know the displays that go with the music. Something like that might work for you as well.Ths is set up for 120VAC because it was meant for lights but I know I saw an LED board set up as a working model of one of these circuits some where.

     

    Here is a link that I came accross if you look around there site they have a program on there to.

     

    http://discolitez.com/pmwiki/pmwiki.php?n=hardware.deluxe32