Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Running a pic18F45K20 at full speed
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 503 subscribers
  • Views 1679 views
  • Users 0 members are here
  • i2c
  • pic18f45k20
  • ds1803
  • pics
Related

Running a pic18F45K20 at full speed

JohnDSiviter
JohnDSiviter over 15 years ago

Can anyone help with this simple problem, I want to achieve full speed 64MHz, at the moment I am getting 16MHz external, when I run a simple while loop (while(1){PORTD=0xFF;PORTD=0x00;}, I get a 4MHz squarewave, also I am having problems getting I2C working communicating with a DS1803E-010DS1803E-010 digital potentiometer:

 


#pragma config FOSC = INTIO7, FCMEN = OFF, IESO = OFF                       // CONFIG1H
#pragma config PWRT = ON, BOREN = OFF, BORV = 30                            // CONFIG2L
#pragma config WDTEN = OFF, WDTPS = 32768                                   // CONFIG2H
#pragma config MCLRE = OFF, LPT1OSC = OFF, PBADEN = OFF, CCP2MX = PORTC     // CONFIG3H
#pragma config STVREN = ON, LVP = OFF, XINST = OFF                          // CONFIG4L
#pragma config CP0 = OFF, CP1 = OFF, CP2 = OFF, CP3 = OFF                   // CONFIG5L
#pragma config CPB = OFF, CPD = OFF                                         // CONFIG5H
#pragma config WRT0 = OFF, WRT1 = OFF, WRT2 = OFF, WRT3 = OFF               // CONFIG6L
#pragma config WRTB = OFF, WRTC = OFF, WRTD = OFF                           // CONFIG6H
#pragma config EBTR0 = OFF, EBTR1 = OFF, EBTR2 = OFF, EBTR3 = OFF           // CONFIG7L
#pragma config EBTRB = OFF                                                  // CONFIG7H

/** I N C L U D E S **************************************************/
#include "p18f45k20.h"
#include "07 ADC.h"  // header file
#include "delays.h"
#include "spi.h"
#include "i2c.h"

//#include "math.h"
//#include "08 Interrupts.h"  // header file ****throws error

/** Prototypes**/
void main(void);
unsigned char I2C_SendByte(char myVolume);//char myByte)
unsigned char IncrementGrey(unsigned char Value); unsigned char DecrementGrey(unsigned char Value);
unsigned char WriteI2C1(  unsigned char data_out );
unsigned char ReadI2C1(  unsigned char data_out );
/** V A R I A B L E S *************************************************/
#pragma udata   // declare statically allocated uinitialized variables

/** D E C L A R A T I O N S *******************************************/
#pragma code    // declare executable instructions

/*******Global Variables******************/

/**********************************/
void main(void)
{
unsigned char count=1;
signed   char Direction_Up=-1;
unsigned char volume=0x00;
unsigned char PA=0x00;
unsigned char NAPA=0x00;
unsigned char greyCode=0x00;
unsigned char temp;
unsigned char PORTx;
/******************************************************************/
WDTCONbits.SWDTEN = 0; // Disable Watchdog
OSCTUNEbits.PLLEN    = 1; // Enable PLL //PLL enabled for INTOSC (4 MHz and 8 MHz only)

// IDLEN IRCF2 IRCF1 IRCF0 OSTS(1) IOFS SCS1 SCS0

OSCCONbits.IDLEN     = 0;    // Not enable pherimetral during sleep()
OSCCONbits.SCS1      = 1;    // Internal oscillator selected
OSCCONbits.SCS0      = 0;    //

OSCCONbits.IRCF2     = 1;    // 16 Mhz selected, 110=8Mhz
OSCCONbits.IRCF1     = 1;
OSCCONbits.IRCF0     = 1;

while(OSCCONbits.OSTS == 0){}       //Oscillator Start-up Time-out Status bit
while(OSCCONbits.IOFS == 0){}       //INTOSC Frequency Stable bit       
/******************************************************************/
    // Init I/O
    TRISC = TRISD = 0x00;      // PORTD bits 7:0 are all outputs (0)
    TRISB = 0xFF;  // PORTB (Encoder) are all inputs (1)
// TRISAbits.TRISA0 = 1;  // TRISA0 input

INTCON2bits.RBPU = 0;  // enable PORTB internal pullups
INTCON = 0b11100000;
INTCONbits.GIEL = 1;
INTCON2bits.INTEDG1 = 0;
INTCON3bits.INT1IP = 0;
INTCON3bits.INT1IE = 1;
INTCON3bits.INT1IF = 0;
//INTCON.PLLEN = 1;
RCONbits.IPEN = 1;

WPUBbits.WPUB0 = 1;   // enable pull up on RB0
    TRISBbits.TRISB0 = 1;       // PORTB bit 0 (connected to switch) is input (1)

PA=NAPA=PORTD=0;
volume=0xFF;PORTD=0xFF;
while(1)
{

PA=NAPA;
/* remove this after test */
while (!Switch_Pin1)
{
  Delay1KTCYx(50); //delay for switch debouncing - triggers lagging edge
  if (Switch_Pin1) {Delay1KTCYx(50);NAPA = IncrementGrey(NAPA);} //Increments PA on key release
}
/**************************/
// NAPA=PORTB;
if (PA!=NAPA)
{
  switch(NAPA)
  {

     case 0x00:
        switch (PA) //check last state
        {
         case 0x02:Direction_Up=1; break;
         case 0x01:Direction_Up=0; break;
         default:  Direction_Up=-1;break;
        }
      break;

      case 0x01:
        switch (PA)
        {
         case 0x00:Direction_Up=1; break;//TEMP STOP CODE break;
         case 0x03:Direction_Up=0; break;
         default:  Direction_Up=-1;break;
        }
      break;

     case 0x03:
        switch (PA)
        {
         case 0x01:Direction_Up=1; break;
         case 0x02:Direction_Up=0; break;
         default:  Direction_Up=-1;break;
        }
      break;
         
      case 0x02:
        switch (PA)
        {
         case 0x03: Direction_Up=1; break;   
         case 0x00: Direction_Up=0; break;
         default:   Direction_Up=-1;break;
        }
      default:break;
    
  }
}

switch (Direction_Up)
{
  case 1: volume++;PORTx = I2C_SendByte(volume);PORTD = volume;break;
    default: break;
  case 0: volume--;PORTx = I2C_SendByte(volume);PORTD = volume;break;
}

Direction_Up=-1;
} //while end

}


unsigned char I2C_SendByte(char myVolume)//char myByte)
{
unsigned char SPI_result=-1;
 
//• MSSP Control Register 1 (SSPCON1)
//• MSSP Control Register 2 (SSPCON2)
//• MSSP STATUS register (SSPSTAT)
//• Serial Receive/Transmit Buffer Register
//(SSPBUF)
//• MSSP Shift Register (SSPSR) – Not directly
//accessible
//• MSSP Address Register (SSPADD)
SSPSTAT = 0x80;//Disable SMBus & Slew Rate Control
SSPCON1 = 0x28; //Enable MSSP Master, SSPCON1=MASTER;
   // SPPADD must go after SSPCON1=MASTER; // ADD<7:0> = 1/Fi2c * FOSC-1 = 1/400,000 * 16,000 - 1 = 39 = 0010,0111b = 0x27
SSPCON2 = 0x00; //Clear Control Bits
//SSPADD = 0x18; //Should be 0x18 for 100kHz
SSPADD=0x27;//SCL pin clock period = ((ADD<7:0> + 1) *4)/FOSC
DDRCbits.RC3 = 1; //Configure SCL as Input
DDRCbits.RC4 = 1; //Configure SDA as Input
   //StartI2C();
   //OpenI2C(MASTER, SLEW_ON);
     SPI_result =WriteI2C(0b10100000);// 0101,address
     Delay1KTCYx(500);
  SPI_result =WriteI2C(myVolume);
  //Delay1KTCYx(500);
  return ReadI2C();
}

 

unsigned char IncrementGrey(unsigned char Value)
{
switch (Value)
{
   case 0x00:Value=0x01;break;
   case 0x01:Value=0x03;break;
   case 0x03:Value=0x02;break;
   case 0x02:Value=0x00;break;
   default:break;
}
return Value;
}
unsigned char DecrementGrey(unsigned char Value)
{
switch (Value)
{
   case 0x00:Value=0x02;break;
   case 0x01:Value=0x00;break;
   case 0x03:Value=0x01;break;
   case 0x02:Value=0x03;break;
   default:break;
}
return Value;
}

  • Sign in to reply
  • Cancel
Parents
  • KennyMillar
    KennyMillar over 15 years ago

    To run at full speed you need to enable the internal HS Oscillator to run at 16Mhz and the x4 PLL

    When running at 64Mhz I don't believe you can have the clock output on pin RA6, but your config (FOSC=INTIO7) has the clock going out on RA6

     

    Unfortunately I am not at my dev machine at the moment, so I can't give you the C Compiler macros you need to use for #pragma config... but I know that it is not INTIO7

    You need to have bits 3 to 0 of register CONFIG1H set to  0110 to enable the 16Mhz internal oscillator AND enable the x4 PLL

    You also need to set bits 5 to 0 in the OSCTUNE register to 011111 t set the internal oscillator to maximum frequency and then bit 6 of OSCTUNE to 1 to enable the PLL

     

    There may well be compiler macros you can use in #pragma config to set all these options for you - but like I say I can't check them for you at the moment.

     

    You should also check out the data sheet (http://ww1.microchip.com/downloads/en/DeviceDoc/41303G.pdf) and look at the registers CONFIG1H and OSCTUNE

     

    I haven't looked at your I2C code yet - but I recently completed a product with PIC18F46K20-E/PPIC18F46K20-E/P and I2C components (oled displays) - but I wrote my own library to do it and bit-banged it out on pins other than the dedicated I2C pins and it worked a treat.

     

    I hope this helps.

     

    Message was edited by: Kenny Millar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • KennyMillar
    KennyMillar over 15 years ago

    To run at full speed you need to enable the internal HS Oscillator to run at 16Mhz and the x4 PLL

    When running at 64Mhz I don't believe you can have the clock output on pin RA6, but your config (FOSC=INTIO7) has the clock going out on RA6

     

    Unfortunately I am not at my dev machine at the moment, so I can't give you the C Compiler macros you need to use for #pragma config... but I know that it is not INTIO7

    You need to have bits 3 to 0 of register CONFIG1H set to  0110 to enable the 16Mhz internal oscillator AND enable the x4 PLL

    You also need to set bits 5 to 0 in the OSCTUNE register to 011111 t set the internal oscillator to maximum frequency and then bit 6 of OSCTUNE to 1 to enable the PLL

     

    There may well be compiler macros you can use in #pragma config to set all these options for you - but like I say I can't check them for you at the moment.

     

    You should also check out the data sheet (http://ww1.microchip.com/downloads/en/DeviceDoc/41303G.pdf) and look at the registers CONFIG1H and OSCTUNE

     

    I haven't looked at your I2C code yet - but I recently completed a product with PIC18F46K20-E/PPIC18F46K20-E/P and I2C components (oled displays) - but I wrote my own library to do it and bit-banged it out on pins other than the dedicated I2C pins and it worked a treat.

     

    I hope this helps.

     

    Message was edited by: Kenny Millar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • JohnDSiviter
    JohnDSiviter over 15 years ago in reply to KennyMillar

    Thanks Kenny, I have set the: #pragma config FOSC = HSPLL, however now the pic doesnt run at all, making me think this is for an external crystal only?  My updated code is:


    /** C O N F I G U R A T I O N   B I T S ******************************/

    #pragma config FOSC = INTIO7, FCMEN = OFF, IESO = OFF                        // CONFIG1H
    #pragma config PWRT = ON, BOREN = OFF, BORV = 30                            // CONFIG2L
    #pragma config WDTEN = OFF, WDTPS = 1                                       // CONFIG2H
    #pragma config MCLRE = OFF, LPT1OSC = OFF, PBADEN = OFF, CCP2MX = PORTC     // CONFIG3H
    #pragma config STVREN = ON, LVP = OFF, XINST = OFF                          // CONFIG4L
    #pragma config CP0 = OFF, CP1 = OFF, CP2 = OFF, CP3 = OFF                   // CONFIG5L
    #pragma config CPB = OFF, CPD = OFF                                         // CONFIG5H
    #pragma config WRT0 = OFF, WRT1 = OFF, WRT2 = OFF, WRT3 = OFF               // CONFIG6L
    #pragma config WRTB = OFF, WRTC = OFF, WRTD = OFF                           // CONFIG6H
    #pragma config EBTR0 = OFF, EBTR1 = OFF, EBTR2 = OFF, EBTR3 = OFF           // CONFIG7L
    #pragma config EBTRB = OFF                                                  // CONFIG7H

    /** I N C L U D E S **************************************************/
    #include "p18f45k20.h"
    #include "07 ADC.h"  // header file
    #include "delays.h"
    #include "i2c.h"

    //#include "math.h"
    //#include "08 Interrupts.h"  // header file ****throws error

    /** Prototypes**/
    void main(void);
    unsigned char I2C_SendByte(char myVolume);//char myByte)
    unsigned char IncrementGrey(unsigned char Value); unsigned char DecrementGrey(unsigned char Value);
    /** V A R I A B L E S *************************************************/
    #pragma udata   // declare statically allocated uinitialized variables

    /** D E C L A R A T I O N S *******************************************/
    #pragma code    // declare executable instructions

    /*******Global Variables******************/

    /**********************************/
    void main(void)
    {

    /******************************************************************/
      //OSCCON*****************
    // IDLEN IRCF2 IRCF1 IRCF0 OSTS(1) IOFS SCS1 SCS0

    OSCCONbits.IDLEN     = 0;    // Not enable pherimetral during sleep()
    //Internal Frequency selection bits
    OSCCONbits.IRCF2     = 1;    // 16 Mhz selected, 110=8Mhz
    OSCCONbits.IRCF1     = 1;
    OSCCONbits.IRCF0     = 1;
    WDTCONbits.SWDTEN    = 0; // Disable Watchdog
    // OSCTUNE***************
    OSCTUNEbits.TUN0  = 1;
    OSCTUNEbits.TUN1  = 1;
    OSCTUNEbits.TUN2  = 1;
    OSCTUNEbits.TUN3  = 1;
    OSCTUNEbits.TUN4  = 1;
    OSCTUNEbits.TUN5  = 0;
    OSCTUNEbits.PLLEN = 1; // Enable PLL //PLL enabled for INTOSC (4 MHz and 8 MHz only)
    OSCTUNEbits.INTSRC= 1;// PLL for 31khz option when selected
      //(SCS)System clock select bits:
    OSCCONbits.SCS0      = 0; //  // Internal oscillator selected
    OSCCONbits.SCS1      = 0;    //
    //scs: 00 = Primary clock (determined by CONFIG1H[FOSC<3:0>]).
    //Clock Status bits:
    while(OSCCONbits.OSTS == 0){}       //Oscillator Start-up Time-out Status bit
    while(OSCCONbits.IOFS == 0){}       //INTOSC Frequency Stable bit       
    /******************************************************************/
        // Init I/O
        TRISD = 0x00;              // PORTD bits 7:0 are all outputs (0)
        TRISB = 0xFF;             // PORTB (Encoder) are all inputs (1)
    TRISC = 0xFF;
    INTCON2bits.RBPU = 0;  // enable PORTB internal pullups
    INTCONbits.GIEL  = 0;
    INTCON2bits.INTEDG1 = 0;
    INTCON3bits.INT1IP = 0;
    INTCON3bits.INT1IE = 1;
    INTCON3bits.INT1IF = 0;
    RCONbits.IPEN = 1;

    WPUBbits.WPUB0 = 1;   // enable pull up on RB0
    /*********************************************************************/
    PA=NAPA=PORTD=0;
    volume=0xFF;PORTD=0x44;

     

    //generate squarewave.....
      while (1){PORTD=0xFF;Nop();Nop();PORTD=0x00;}
    }

     

     

    The code above generates a 16Mhz signal on RA6 (as expected: 64Mhz/4=16Mhz), but the squarewave output is just 2,7Mhz??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 15 years ago in reply to JohnDSiviter

    Hi John,

     

    In order to narrow down your problem, I suggest you first write a very simple program that blink an LED every second based on a timer.

    This will help making your hardware stable.

     

    Can you post your board schematic or give a link if it is an existing commercial board ?

    What is your Vdd ?

    Did you put some capacitors around your oscillator ? which value ?

    How about your Reset circuit ?

    How do you program your PIC ?

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JohnDSiviter
    JohnDSiviter over 15 years ago in reply to MicrochipRTCfr

    Hi, I am using the 44-pin pickit development board with the said processor which has decoupling capacitors on there I believe, I am using the ICD3 with it however.

     

    The program works, except for getting a 64Mhz clock, I have extracted the configuration lines to make it easier for you:

     

    /** C O N F I G U R A T I O N   B I T S ******************************/

    #pragma config FOSC = INTIO67, FCMEN = OFF, IESO = OFF                        // CONFIG1H

     

    void main(void)
    {

    WDTCONbits.SWDTEN    = 1; // Disable Watchdog
    // OSCTUNE***************
    OSCTUNEbits.TUN1  = 1;
    OSCTUNEbits.TUN2  = 1;
    OSCTUNEbits.TUN3  = 1;
    OSCTUNEbits.TUN4  = 1;
    OSCTUNEbits.TUN5  = 1;
    OSCTUNEbits.PLLEN = 1; // Enable PLL //PLL enabled for INTOSC (4 MHz and 8 MHz only)
    OSCTUNEbits.INTSRC= 1;
    //OSCCON*****************
    // IDLEN IRCF2 IRCF1 IRCF0 OSTS(1) IOFS SCS1 SCS0

     

    OSCCONbits.IDLEN     = 0;    // Not enable pherimetral during sleep()
    //Internal Frequency selection bits
    OSCCONbits.IRCF2     = 1;    // 16 Mhz selected, 110=8Mhz
    OSCCONbits.IRCF1     = 1;
    OSCCONbits.IRCF0     = 1;
    //CONFIG1H = 6;
      //(SCS)System clock select bits:
    OSCCONbits.SCS0      = 1; //  // Internal oscillator selected
    OSCCONbits.SCS1      = 0;    //
    //scs: 00 = Primary clock (determined by CONFIG1H[FOSC<3:0>]).
    //Clock Status bits:
    while(OSCCONbits.OSTS == 0){}       //Oscillator Start-up Time-out Status bit
    while(OSCCONbits.IOFS == 0){}       //INTOSC Frequency Stable bit       
    /******************************************************************/
        // Init I/O
        TRISD = 0x00;              // PORTD bits 7:0 are all outputs (0)
        TRISB = 0xFF;             // PORTB (Encoder) are all inputs (1)
    TRISC = 0xFF;
    INTCON2bits.RBPU = 0;  // enable PORTB internal pullups
    INTCONbits.GIEL  = 0;
    INTCON2bits.INTEDG1 = 0;
    INTCON3bits.INT1IP = 0;
    INTCON3bits.INT1IE = 1;
    INTCON3bits.INT1IF = 0;
    RCONbits.IPEN = 1;

    WPUBbits.WPUB0 = 1;   // enable pull up on RB0

     

      while (1){PORTD=0xFF;Nop();Nop();PORTD=0x00;}

    }

    Not sure why you wish to see my circuit as I am using the internal oscillator, however its no different to the original demo board for the PIC18F45K20-I/MLPIC18F45K20-I/ML except for the addition of a Dallas DS1803E-010DS1803E-010 digital potentiometer wired into the I2C.

    I program using an ICD3 with interface adaptor to 6 pin header.

    The circuit should be fine, maybe I need a decoupling cap close to the DS1803E-010DS1803E-010 come to think of it, I am planning to use internal pullups on the I2C interface, but hey all I wanna know is how do you set up a PIC18F45K20-I/MLPIC18F45K20-I/ML to run code at max speed and give me a result I can see on a scope, answer in C18 please image