Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Suggest a project for me
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 32 replies
  • Subscribers 506 subscribers
  • Views 3023 views
  • Users 0 members are here
  • c
  • project
  • mbed
  • multicomp
  • electronics
  • amicus
  • arduino
Related

Suggest a project for me

awinning
awinning over 16 years ago

Hi,

 

I've really enjoyed being on element14, and it has reawakened my desire to actually play around with electronics. I think the main spur has been reading about the Arduino like boards coming onto the market now. At the moment we have three Multicomp Arduino clone boards here, the Amicus board, which is an Arduino clone with a PIC controller here, and mbed. I think personally I'd like to try the PIC programming, but if anyone thinks the AVR or mbed is easier to get into, I'm open to convincing.

 

About me,

I graduated in 1996 with a BSc in Electronic Systems. Since then I have worked in a number of publications writing about electronics, but not practising. My favourite subjects were digital design and C programming. Currently I'm working on this, which hopefully you are all familiar with.

 

About the project,

I'm looking for something to ease me back into electronics. I want to use either one of the Arduino clone boards or an mbed. I'd hopefully be designing a shield/board for the chosen dev kit using EAGLE Freemium. The project should be fairly cheap and at an intermediate level, I'd like to stretch myself a bit while learning (and hopefully you are all going to help me through image).

 

Any and all suggestions welcome!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Is there a particular reason for using the EAGLE Freemium? Why don't you start over with the Freeware version? OK, you're bound to two signal layers only, but do you really need more for the first run? And yes, you're also limited to one schematic sheet. But there is no limit for the sheet's size. On the other hand, the Freeware does not require registration, does need a internet connection, is not limited to one computer and, most impotant, does not stop working after 60 days.

     

    If you need more power somewhen (more schematic sheets, more signal layers, more board space), you can get the Standard version for hobbyists, see http://www.cadsoft.de/nonprofit.htm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    Is there a particular reason for using the EAGLE Freemium? Why don't you start over with the Freeware version? OK, you're bound to two signal layers only, but do you really need more for the first run? And yes, you're also limited to one schematic sheet. But there is no limit for the sheet's size. On the other hand, the Freeware does not require registration, does need a internet connection, is not limited to one computer and, most impotant, does not stop working after 60 days.

     

    If you need more power somewhen (more schematic sheets, more signal layers, more board space), you can get the Standard version for hobbyists, see http://www.cadsoft.de/nonprofit.htm