Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Overcurrent protection, what is a cheap and simple way
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 503 subscribers
  • Views 1068 views
  • Users 0 members are here
  • embedded
  • Design
  • development
Related

Overcurrent protection, what is a cheap and simple way

Catwell
Catwell over 15 years ago

I hope this message gets read....

 

 

 

In a circuit I am working on, I am powering two pins at the same time. These pins are powering a single LED.

When I power both pins I am doubling the current powering an LED.

 

What I need to do is protect the LED from excess amperage. What suggestions do you have? I know there are many ways of doing the same thing, I just want to collect them all.

 

Any help would be appreciated.

 

Cabe

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    High Cabe,

     

    If you want to have a controlled current source to drive an LED, which accommodates supply voltage variation and could be driven by more than one signal, that's easy.  You could do this with two transistors and 2 to 4 resistors (and 2 diodes if you need to control with two signals).  Unsure on the requirements.  It's also possible to use only one transistor, given the control signal is referenced to a regulated power supply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Catwell
    Catwell over 15 years ago in reply to e14 Contributor

    Eclipze,

     

    I like where your head is at on this obstacle.

     

    Could you post a possible circuit of your idea?

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Catwell

    Hi Cabe,

     

    I don't have enough information about the circuit you have.  You have 2 pins powering a single LED.  But I don't know what type of signals these pins have. It's better if you can define what you need to acheive, along with the systems contraints.  What's the power supply, is it regulated, what current are you targeting, what are the two controlling signals... 5V, 3V, a push button or switch etc...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Catwell

    Hi Cabe,

     

    I don't have enough information about the circuit you have.  You have 2 pins powering a single LED.  But I don't know what type of signals these pins have. It's better if you can define what you need to acheive, along with the systems contraints.  What's the power supply, is it regulated, what current are you targeting, what are the two controlling signals... 5V, 3V, a push button or switch etc...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Catwell
    Catwell over 15 years ago in reply to e14 Contributor

    Eclipze,

     

    Input voltages on both pins from an unregulated supply (no clue what it is, to be honest):

    Pin 1 :14.5V

    Pin 2 :14.5V

     

    Current on the LED should be 20mA.

     

    Normally, one one of the pins will be on, and the system will be fine. But my customers are not quite sure what they are doing, and might power both pins at the same time.

     

    I have limited space on my circuit board, and need a small, simple solution. Possibly close to the LED itself after the point where both inputs combine.

     

    Thoughts?

     

    Cabe