Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Overcurrent protection, what is a cheap and simple way
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 503 subscribers
  • Views 1068 views
  • Users 0 members are here
  • embedded
  • Design
  • development
Related

Overcurrent protection, what is a cheap and simple way

Catwell
Catwell over 15 years ago

I hope this message gets read....

 

 

 

In a circuit I am working on, I am powering two pins at the same time. These pins are powering a single LED.

When I power both pins I am doubling the current powering an LED.

 

What I need to do is protect the LED from excess amperage. What suggestions do you have? I know there are many ways of doing the same thing, I just want to collect them all.

 

Any help would be appreciated.

 

Cabe

  • Sign in to reply
  • Cancel
Parents
  • jvdberg@ieee.org
    jvdberg@ieee.org over 15 years ago

    The easiest way is to put a resistor in series with the led. 14.5 Volt / 20 mA = 0.725 kiloohm.

    A 750 ohm resistor will do. If the outputs have a current control for the LED, the current now only will be limited by the resistor. If the output currents are limited with an internal resistor, the total resistance will be higher, resulting in a different brightness when two outputs are driving the LED. The maximum current however will not be exceeded. In that case a lower resistor value can be used, so in case of two outputs are driving the LED, the maximum current will not be exceeded.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jvdberg@ieee.org
    jvdberg@ieee.org over 15 years ago

    The easiest way is to put a resistor in series with the led. 14.5 Volt / 20 mA = 0.725 kiloohm.

    A 750 ohm resistor will do. If the outputs have a current control for the LED, the current now only will be limited by the resistor. If the output currents are limited with an internal resistor, the total resistance will be higher, resulting in a different brightness when two outputs are driving the LED. The maximum current however will not be exceeded. In that case a lower resistor value can be used, so in case of two outputs are driving the LED, the maximum current will not be exceeded.