Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Steam powered turntable controlled with Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 502 subscribers
  • Views 378 views
  • Users 0 members are here
  • microchip
  • 16_bit
  • microprocessor
  • robots
  • microcontrollers
  • microcontroller
  • steampunk
  • arduino
Related

Steam powered turntable controlled with Arduino

Catwell
Catwell over 15 years ago
image
 
Steampunk themed inventions have been around for a while now but this turn table stands out among the best of them. Simon Jansen from Auckland, New Zealand designed his turntable using a miniature boiler and an Arduino unit. He describes the process he used to achieve this, “The engine was made mainly from bits and pieces I had lying about in my junk box. The boiler was made from some copper water pipe and a bespoke platter and base was made using wood. I am using an Arduino to control everything buy using a coil to detect the passing of magnets in the edge of the platter. The Arduino works out the revs then feeds this information into a PID controller the output of which drives a servo controlling a throttle on the engine. The speed is regulated to 33 1/3 (well, more or less) and displayed on an analogue meter. The tone arm uses an old phono cartridge that connects to my phono pre-amp and into my stereo. The hardware is complete and works well but the software could use a little tweaking. It does however run!” As he built this primarily to play the Sex Pistols on, it is indeed steampunk in the truest sense of the word. To see a complete detailed process on how he made everything (even the Arduino) please visit: http://www.asciimation.co.nz/bb/2010/11/30/a-steam-punk-record-player

Cabe