Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum IBM unveils electrical and optical devices on one chip
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 502 subscribers
  • Views 540 views
  • Users 0 members are here
  • embedded
  • light_computing
  • Design
  • photonic_computing
  • development
Related

IBM unveils electrical and optical devices on one chip

Catwell
Catwell over 15 years ago
image
 
Computer processors are kind of like Steve Austin (the bionic man); they become smaller, faster, better. However unlike Steve, processors will still be used in some form or another long after today’s become obsolete. They actually will become faster and more efficient, well according to IBM they will. The company has recently unveiled a new chip that combines electrical and optical devices on the same chip. Called CMOS integrated Silicon Nanophotonics, the chip incorporates Nanophotonics that enable the chip to communicate using pulses of light rather than electrical signals. Dr. T.C. Chen, vice president of Science and Technology at IBM Research says that, “The development of the Silicon Nanophotonics technology brings the vision of on-chip optical interconnections much closer to reality, with optical communications embedded into the processor chips, the prospect of building power-efficient computer systems with performance at the Exaflop level is one step closer to reality.” An Exaflop super computer can perform one million trillion calculations a second. That’s considerably faster than anything in use today. Then new technology can be made using the standard CMOS process and doesn’t need any special tooling to do so. To do this researchers at IBM have made a suite of compact active and passive silicon nanophotonics that are scaled down to the smallest size that dielectric optics can be at this point. I wonder how much heat is generated when these chips are running at full potential. More here :http://www-03.ibm.com/press/us/en/pressrelease/33115.wss

Cabe
 
Picture from IBM's website, rights there of
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    There's been talk of using optics on silicon for decades now. Good to see it actually implemented and perhaps becoming feasible. IBM are certainly not the only company interested in this technology, for example Intel are pursuing this tech too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    There's been talk of using optics on silicon for decades now. Good to see it actually implemented and perhaps becoming feasible. IBM are certainly not the only company interested in this technology, for example Intel are pursuing this tech too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Catwell
    Catwell over 15 years ago in reply to e14 Contributor

    Grimrob,

     

    Intel has already produced a light based, high bandwidth, connection between devices/components. Nano scale lasers are already in the die with Intel's Light Peak, based on the Photonics Link they developed a while ago.

     

    When they reach the interconnect level, they will be a boom in technology advancement for sure. Moving data from semi-conductor networks, a CPU lets's say, elsewhere needs to operate faster, and these light based connections are the most likely to happen compared to other solutions.

     

    I see I have been following this closely.

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Catwell

    Ah, thanks for the links. Didn't realise it had been posted about already. I really fancy the idea of my computer communicating using light someday - kinda stuff of the future image Any fundamental changes in technology are always very exciting.