Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Plug-and-play Modules for Prototyping: ST Launches Third-Generation Dev Platform for STM8 and STM32
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 503 subscribers
  • Views 316 views
  • Users 0 members are here
  • stmicroelectronics
  • evoprimer
Related

Plug-and-play Modules for Prototyping: ST Launches Third-Generation Dev Platform for STM8 and STM32

GardenState
GardenState over 15 years ago

image


STMicroelectronics hopes to simplify product design with the new EvoPrimer platform plug-and-play modules for prototyping with the STM8 and STM32 MCUs.

The third generation platform builds on experience from ST’s Primer and Primer2 kits. Now, EvoPrimer further increases flexibility and lowers customers’ overall investment in tools by providing a common base unit with interchangeable low-cost microcontroller modules, or target boards..

Target boards are available now to support STM8L 8-bit microcontrollers, as well as the 32-bit STM32F Connectivity and Performance Lines families. Additional target boards are soon to be introduced for the STM32L and the STM32 F-2 series featuring 90nm process technology.

The EvoPrimer is initially available as a kit with one specified target board, priced at $99. Extra target boards are available for $24, and the base unit can also be purchased separately for $75. The platform is shipped with the Raisonance Ride 7 application development environment, and the Raisonance STM8 C compiler or GNU C compiler for STM32.

The target boards connect readily to functions on board the EvoPrimer base unit, including an LCD touchscreen, a joystick, a MEMS accelerometer, a microphone, loudspeaker and jack, a Micro SD card connector, and a Li-ion battery with charge-management circuitry. An integrated extension connector allows extra functions to be added, if needed. EvoPrimer is also integrated with the CircleOS operating system, which provides services that save designers having to understand all the complexities of the MCU.

To help users ST supports two online communities (www.stm8circle.com  and www.stm32circle.com) bringing together engineers using Primer tools with the STM8 or STM32 families. Almost 100 downloadable projects are available to members, and most will run immediately on EvoPrimer.

  • Sign in to reply
  • Cancel
Parents
  • firatkocak
    firatkocak over 15 years ago

    I already have a primer2 kit and i am very happy with it. But EvoPrimer is a far step as much as i can see. It would be great to have one ...

     

    Firat Kocak

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • firatkocak
    firatkocak over 15 years ago

    I already have a primer2 kit and i am very happy with it. But EvoPrimer is a far step as much as i can see. It would be great to have one ...

     

    Firat Kocak