Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum First floating-point microcontroller for extreme temperatures
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 502 subscribers
  • Views 757 views
  • Users 0 members are here
  • high-temperatures
  • mcu
  • ti
Related

First floating-point microcontroller for extreme temperatures

GardenState
GardenState over 15 years ago

 
Texas Instruments has introduced what it says is the industry's first floating-point microcontroller (MCU) for extreme temperature operation (from -55 degrees Celsius to 210 degrees Celsius). Exceeding the traditional 150 degrees Celsius limit for other high-temperature semiconductors, the SM320F28335-HT Delfino 32-bit MCU is designed for manufacturers of electronics operating in harsh and hot environments, such as downhole drilling, commercial jet engines, motor control, military applications, and medical instruments and surgical tools requiring sterilization.
 
The SM320F28335-HT Delfino MCU is based on TI's TMS320C2000 MCU platform, which combines control peripheral integration and embedded flash memory with the processing power of a 32-bit floating-point architecture. Enabling operation at up to 210 degrees Celsius eliminates the need for expensive up-screening and qualification tests of industrial grade MCUs, allowing for faster design of applications operating in harsh environments and cutting development time by up to one year, according to TI.
 
The TMS320F28335 Experimenter Kit, which is based on the commercial grade, code-compatible version of the F28335 Delfino MCU, is also immediately available for experimentation and code development for the new high-temperature version. The kit is priced at $99.
 
The device is available in a hermetic ceramic pin grid array package. Pricing is $406.25 in 100-unit quantities.

  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB over 15 years ago

    Do you have a link to the web site?

    Thanks

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Eavesdropper
    Eavesdropper over 15 years ago in reply to DAB

    DAB,

     

    Googled it on T.I.'s site. http://focus.ti.com/docs/prod/folders/print/sm320f28335-ht.html

     

    Amazing temperature resiliance, I must say.

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 15 years ago in reply to Eavesdropper

    Thanks

    They have a very complete web site for the product.  One thing I did not see though was a current use verses temperature chart.  I may do some searching to see what I can find, but this thing looks really interesting.

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 15 years ago in reply to Eavesdropper

    Thanks

    They have a very complete web site for the product.  One thing I did not see though was a current use verses temperature chart.  I may do some searching to see what I can find, but this thing looks really interesting.

    DAB