Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum External memory Flash SPI
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 502 subscribers
  • Views 1441 views
  • Users 0 members are here
Related

External memory Flash SPI

e14 Contributor
e14 Contributor over 15 years ago

Hello,

 

We've worked with an Atmel Flash Memory but we met some problem to Write and Read data ( explained in the post : Read / Write on Atmel Flash in Embedded Design). And even when we do a read Manufacturer and Devide ID, it didn't answer the good information.

 

Does anyone has already used a SPI memory ? Which kind of memory, easy to use, would you recommend ? Which memory is the most used ?

 

Thank you.

 

Regards.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hello Michael,

     

    Thank you for your answer. The Atmel memory we've used is an AT25DF041A-SSH-BAT25DF041A-SSH-B and AT25DF081A. In their datasheet it's written :

    • Single 2.3V - 3.6V or 2.7V - 3.6V Supply

    So with 3.3V it should be OK.

    The memory we've choosen is a SOP8 and is correct for our application but it didn't answer correctly to our SPI request....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 15 years ago in reply to e14 Contributor

    Sorry - confusion between A part and part non A part.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 15 years ago in reply to michaelkellett

    I should have clarified that I used Microcchip 23K256 which is Vcc 2.7 to 3.3V.  There is the lower power version: 23A256.

     

    Michael Kellett - I'm in the US and had been looking at Newark & element14 Store.  I don't recall seeing that large of SPI RAM.  It seemed like the only option above couple hunderd Kb was parallel.  I'd love a 4Mbit serial memory! Could you post some part numbers?

     

     

    [Background on my project which got put on-hold: I wanted to delay radio broadcast to sync up with digital cable TV for football games since I like the local play-by-play announcers on the radio versus national TV broadcast.  Radio is up 10 seconds ahead of the TV so I wanted to ADC the audio, store in buffer in RAM, read from the buffer for PWM output. 

     

    I was using Arduino and Microchip 256Kbit SRAM (32KB).  I discovered, that even at really low sample rate for the audio, the single 32KB could only provide 1-2 seconds buffering.  I had thought of adding more chips to the SPI bus but hadn't tried. 

     

    I also ordered this CPLD shield for Arduino, Amani64, but haven't tried it yet.  It could be used to offload the complexity of addressing multiple SPI RAM chips:  http://majolsurf.net/wordpress/?page_id=1001]

     

     

    Cheers,

    Drew

    http://twitter.com/pdp7

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 15 years ago in reply to fustini

    Hello Drew,

    Lanzini and I are talking about SPI Flash memory not RAM - I don't know any serial RAMs anything like big enough. I had a quick look at the Amani64 but it seems very limited - only 64 register cpld. Have a look at the Lattice LCMXO2280-B-EVN, complete board with programmer for XO-2280 for $29. Enough FPGA to make an SDRAM controller with an SPI interface.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 15 years ago in reply to fustini

    Hello Drew,

    Lanzini and I are talking about SPI Flash memory not RAM - I don't know any serial RAMs anything like big enough. I had a quick look at the Amani64 but it seems very limited - only 64 register cpld. Have a look at the Lattice LCMXO2280-B-EVN, complete board with programmer for XO-2280 for $29. Enough FPGA to make an SDRAM controller with an SPI interface.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • fustini
    fustini over 15 years ago in reply to michaelkellett

    D'oh! I might be due for a new glasses Rx.  Sorry for the confusion.  Thanks for the Lattice tip - I had been wondering about how I could do SDRAM.

     

    Thanks,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 15 years ago in reply to fustini

    Hi,

     

    You can also find 4MB & even 8MB SPI Flash from SST (2.7V to 3.6V) @ 80MHz :

    http://www.microchip.com/ParamChartSearch/chart.aspx?branchID=71201&mid=&lang=en

     

    regards