Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Altium and Würth Elektronik collaborate on new component libraries
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 502 subscribers
  • Views 455 views
  • Users 0 members are here
  • wuerth
  • components
  • hobart
  • altiumlive
  • emc
  • library
  • würth
  • ferrite
  • elektronik
  • transformers
  • rf
  • component
  • inductors
  • vault
Related

Altium and Würth Elektronik collaborate on new component libraries

PRismaPR
PRismaPR over 15 years ago

Altium and Würth Elektronik collaborate on new component libraries

More than 1,500 passive components from Würth Elektronik available through AltiumLive

 

KARLSRUHE, Germany – 22 June 2011 – Altium announces a comprehensive set of passive components from Würth Elektronik is available for Altium Designer 10 through the recently launched AltiumLive portal. Electronic designers will have access to eight new libraries comprising over 1,500 passive components provided by one of the leaders of EMC solutions for the electronics industry.

 

Würth Elektronik is Europe's largest manufacturer of EMC components, inductors, transformers, RF components and circuit protection devices. In a close collaboration between its passive components unit and Altium, they developed and prepared a full set of libraries for Würth Elektronik’s passive components that is ready to use within Altium Designer. All components in the Würth Elektronik libraries include the schematic symbol, the PCB footprint and a detailed 3D model for 3D mechanical integration during PCB design.

 

Frank Krämer, Technical Marketing Director for Altium in EMEA, commented, “Altium is moving into a new model of partnership to provide third party libraries, templates, reference designs and other ready-to-use IP for our Altium Designer users. I believe this close collaboration between Altium and parts manufacturers will produce design IP that our customers can trust ‘out-of-the-box’, and adds significant value to being a member of the Altium design community. I am happy that we have Würth Elektronik on board to provide easy access to its high quality EMC components from the heart of Europe to our worldwide user base.”

 

Würth Elektronik’s Product Manager Christin Zierenner said, “We are happy to work closely and in partnership with Altium, because our customers are now able to easily access and re-use quality models for our components in the design process”.

 

Altium's collaboration with Würth Elektronik will extend beyond the initial component releases. The ongoing relationship will see the Würth Elektronik inventory kept up to date within the Altium vaults. As new parts are added or components updated in Würth Elektronik's catalogue, they will also be added or modified in the Altium vault. As parts are made obsolete, these parts will be marked as such in the vault. This will give Altium customers an almost 'real-time' insight into the Würth Elektronik component inventory, allowing more intelligent part decisions to be made during board design.

 

The libraries from Würth Elektronik will be available through Altium’s ‘Hobart Vault’, one of Altium’s managed library repositories of ready-to-use design components accessible through the AltiumLive portal. Altium Designer 10 users can access these components by connecting to the Hobart Vault directly from within their Altium Designer software using their AltiumLive credentials, or by browsing to the AltiumLive Design Content area and selecting the Altium Hobart Vault.

 

The library suite provides a choice of eight families of various passive components for different areas of applications comprising:

• EMC ferrites

• Filter inductors

• Common mode line filters

• Common mode power line chokes

• SMD power chokes

• THT power chokes

• Double chokes

• SMD high current chokes

 

The first two libraries to be released into the Hobart Vault are the EMC Ferrite and Filter Inductor families with additional families to follow on a weekly basis.

 

The EMC Ferrite library provides SMD ferrites, SMD ferrites for HF applications, VHF chokes, a kind of ‘choke array’ with a ferrite bridge and flat wire high current SMD ferrites as well as SMD power ferrites. The EMC ferrites are based on a nickel-zinc material mixture. In a frequency range starting with 20MHz, the core material is optimized for small Q factors (Q <3) which equals to high loss. These occur in the core material and help to absorb electromagnetic interferences. The inductance of these components is kept low. The special miniature SMD multilayer ferrites have very good filtering properties and a low DC resistance. Placed close to the current source, maximum impedances of 1,000 Ohms can be achieved. The modified internal structure in the HF variant increases the effective bandwidth to eliminate interference to an extent that impedances at 3GHz are at least three times bigger. The usage of the ferrite bridge can be customized to either implement a dual current-compensated choke or to increase the impedance or the rated current.

 

The Filter Inductor library provides SMD multilayer inductors (0603-1206) and rod core chokes. With their compact design, multi-layer inductors achieve a small DC resistance. The external ferrite casing provides a magnetic shield, signal interference and crosstalk is reduced significantly. The device is particularly suited as in filters and resonant circuits, where low coupling and small packages are required. The rod core choke is not shielded and available in larger packages. The advantage of this design is the broad attenuation and the current capacity, up to 15A. Furthermore, this series is characterized by its high mechanical stability and an operating temperature range from -40 °C to +150 °C.

 

All components are available from Würth Elektronik ex stock. Samples are available free of charge. More info at www.we-online.de.

 

More information on the libraries and how to use them in Altium Designer is available in AltiumLive and in the related blogs.

 

 

Contacts:

Frank Krämer

Altium Europe GmbH

+49 721 8244 108

frank.kraemer@altium.com

 

Gabriele Amelunxen

PRismaPR

+49 8106 247 233

info@prismapr.com

 

Monika Cunnington

PRismaPR (UK)

+44-1462 640 779

monika@prismapr.com

www.prismapr.com

 

About Altium Altium Limited (ASX:ALU) creates electronics design software based on the belief that anyone who wants to create electronic products that make a difference should be able to do so. Altium’s unified electronics design environment links all aspects of electronics product design in a single application that is priced to be as affordable as possible. This helps electronics designers break down barriers to innovation, harness the latest devices and technologies, manage their projects across broad design ‘ecosystems’, and create connected, intelligent designs.

 

Founded in 1985, Altium has headquarters in Sydney, and operates worldwide. For more information, visit www.altium.com.

 

Altium, Altium Designer, LiveDesign and Morfik, and their respective logos, are trademarks or registered trademarks of Altium Limited, or its subsidiaries. All other registered or unregistered trademarks mentioned in this release are the property of their respective owners, and no trademark rights to the same are claimed.

 

About Würth Elektronik eiSos: Würth Elektronik eiSos designs, manufactures and distributes passive and electromechanical components for the electronic industry and runs its own business units in most European countries, in the US, Asia and South America.

Production plants in Europe, Asia and America deliver to a worldwide growing customer base. The offering of Würth Elektronik eiSos includes EMC components, inductors, transformers, RF components & circuit protection, connectors, power supply components, switches and joining technology. Würth Elektronik eiSos is the biggest manufacturer of passive components in Germany.