Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Superconductor Logic Goes Low-Power
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 502 subscribers
  • Views 294 views
  • Users 0 members are here
  • logic
  • exaflop
  • rql
  • superconductor
  • josephson
  • rfsfq
Related

Superconductor Logic Goes Low-Power

squadMCU
squadMCU over 15 years ago

Transistor-based semiconductors have dominated the computing industry since its start. But a much more exotic, transistor-less option has long been lurking in the wings. Superconducting circuits, which boast resistance-less wires and ultrafast switches, can perform the tasks that silicon-based systems do in a fraction of the time.
Now new logic designs are emerging that suggest superconducting processors could be not only faster but also tens or even hundreds of times as energy efficient as their CMOS cousins. And these processors could provide a much-needed path to the next generation of supercomputers, proponents say.
This next generation, called exaflop computers, would be capable of executing a quintillion (1018) operations per second, about 1000 times as many as existing computers can. Once thought to be just 5 or 10 years away, they now seem nearly impossible. A recent estimate suggests that an exascale supercomputer built using CMOS technology would consume some 500 megawatts—the output of a modest nuclear power plant. "What everybody's shooting for is to be able to overturn [that] result," says Erik DeBenedictis of Sandia National Laboratories, in Albuquerque. "Now there's a glimmer of light that it might happen."

Transistor-based semiconductors have dominated the computing industry since its start. But a much more exotic, transistor-less option has long been lurking in the wings. Superconducting circuits, which boast resistance-less wires and ultrafast switches, can perform the tasks that silicon-based systems do in a fraction of the time.

 

Now new logic designs are emerging that suggest superconducting processors could be not only faster but also tens or even hundreds of times as energy efficient as their CMOS cousins. And these processors could provide a much-needed path to the next generation of supercomputers, proponents say.

 

This next generation, called exaflop computers, would be capable of executing a quintillion (1018) operations per second, about 1000 times as many as existing computers can. Once thought to be just 5 or 10 years away, they now seem nearly impossible. A recent estimate suggests that an exascale supercomputer built using CMOS technology would consume some 500 megawatts—the output of a modest nuclear power plant. "What everybody's shooting for is to be able to overturn [that] result," says Erik DeBenedictis of Sandia National Laboratories, in Albuquerque. "Now there's a glimmer of light that it might happen."

 

 

Read the complete entry at Spectrum Magazine

  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB over 15 years ago

    I think the real impediment to superconducting circuits has been their ability to work a room temperature.  Even forty years ago we knew that they could work a very low currents.  The challenge has always been to get a reasonable gain in current reduction with inexpensive materials that did not need a huge facility to pull the temperature down.

     

    Still, it is a step in the right direction.  It will be interesting to see what they can do speed wise and how robust the application can be in real world implementations.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 15 years ago

    I think the real impediment to superconducting circuits has been their ability to work a room temperature.  Even forty years ago we knew that they could work a very low currents.  The challenge has always been to get a reasonable gain in current reduction with inexpensive materials that did not need a huge facility to pull the temperature down.

     

    Still, it is a step in the right direction.  It will be interesting to see what they can do speed wise and how robust the application can be in real world implementations.

     

    DAB