Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Have a question about Micrium's embedded software? Ask our Expert, Matt Gordon
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 502 subscribers
  • Views 4520 views
  • Users 0 members are here
  • applications
  • device
  • embedded
  • kernel
  • micrium
Related

Have a question about Micrium's embedded software? Ask our Expert, Matt Gordon

e14 Contributor
e14 Contributor over 15 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Embedded in the element14 Community Embedded group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

image

 

Matt Gordon

Matt Gordon is a senior applications engineer at Micrium.  He began his career developing device drivers, kernel ports, and example applications for Micrium's customers.  Drawing on this experience, Matt has written multiple articles on embedded software.  He also heads Micrium's training program and regularly teaches classes on real-time kernels and other embedded software components.  Matt holds a bachelor's degree in computer engineering from Georgia Tech, Georgia in the USA.


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Dear Matt, I have a hardware platform based in the ATMEGA 2560 16AU. I wonder if the micrium uC_OS can be ported for that micro?

    Regards

    Cristian Barros

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Cristian,

     

    Yes, Micrium's engineers have already ported uC/OS-II to the ATmega2560.  You can download an example project that incorporates their port files (along with the full source code of the kernel) from the knode: http://www.element14.com/community/docs/DOC-37677/l/project--μcos-ii-and-μcos-view-for-atmel-avr-atmega2560.

     

    Regards,

     

    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Matt,

    Does uC/OS-III support co-operative multitasking i.e. a task can run without interruption until it suspends itself?

    Regards,

    Peter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Peter,

     

    uC/OS-III is a preemptive kernel, so the possibility generally exists that one task might interrupt another.  However, application code ultimately decides whether or not preemption takes place.  If an application's ISRs never invoke kernel functions to ready tasks, then those ISRs will not result in preemption.  Likewise, if the kernel's own ISR, the tick interrupt handler, does not ready any tasks (which should happen if application code avoids using the kernel's time-delay and time-out services), then it will not cause tasks to preempt each other.  Cooperative behavior, then, can be brought about with uC/OS-III, but is not typical of applications that incorporate the kernel.  

     

    Regards,

     

    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Peter,

     

    uC/OS-III is a preemptive kernel, so the possibility generally exists that one task might interrupt another.  However, application code ultimately decides whether or not preemption takes place.  If an application's ISRs never invoke kernel functions to ready tasks, then those ISRs will not result in preemption.  Likewise, if the kernel's own ISR, the tick interrupt handler, does not ready any tasks (which should happen if application code avoids using the kernel's time-delay and time-out services), then it will not cause tasks to preempt each other.  Cooperative behavior, then, can be brought about with uC/OS-III, but is not typical of applications that incorporate the kernel.  

     

    Regards,

     

    Matt