Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Have a question about Micrium's embedded software? Ask our Expert, Matt Gordon
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 502 subscribers
  • Views 4565 views
  • Users 0 members are here
  • applications
  • device
  • embedded
  • kernel
  • micrium
Related

Have a question about Micrium's embedded software? Ask our Expert, Matt Gordon

e14 Contributor
e14 Contributor over 15 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Embedded in the element14 Community Embedded group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

image

 

Matt Gordon

Matt Gordon is a senior applications engineer at Micrium.  He began his career developing device drivers, kernel ports, and example applications for Micrium's customers.  Drawing on this experience, Matt has written multiple articles on embedded software.  He also heads Micrium's training program and regularly teaches classes on real-time kernels and other embedded software components.  Matt holds a bachelor's degree in computer engineering from Georgia Tech, Georgia in the USA.


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi Matt,

     

    Hey I have another evalboard form Luminary Micro LM3S3748-IQC50-A0LM3S3748-IQC50-A0 and Iwant to use the OS-III on this board but the ports for this board are not available for using with OS-III. It is supported with OS-II though. What do you suggest that i should do?

     

    Thanks in advance Matt.

     

    Regards,

    jumbowat

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Technically, just one uC/OS-III port is used for all of the Luminary Micro/TI Stellaris parts; it is a generic Cortex-M3 port.  To run uC/OS-III on the particular board that you have in mind, you will need the kernel's source code and this port.  You will also need a modicum of BSP and application code.  You can get the kernel code (source and port) from an existing uC/OS-III Stellaris project--for instance, the LM3S9B92-based project that was developed for the TI version of Micrium's uC/OS-III book.  You can also borrow your application code from such a project, but this code might need to be modified slightly to suit your platform.  As for the BSP, you should be able to reuse the code from the uC/OS-II project that you mentioned.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thank you Matt. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thank you Matt. image