Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Have a question about Micrium's embedded software? Ask our Expert, Matt Gordon
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 502 subscribers
  • Views 4534 views
  • Users 0 members are here
  • applications
  • device
  • embedded
  • kernel
  • micrium
Related

Have a question about Micrium's embedded software? Ask our Expert, Matt Gordon

e14 Contributor
e14 Contributor over 15 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Embedded in the element14 Community Embedded group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

image

 

Matt Gordon

Matt Gordon is a senior applications engineer at Micrium.  He began his career developing device drivers, kernel ports, and example applications for Micrium's customers.  Drawing on this experience, Matt has written multiple articles on embedded software.  He also heads Micrium's training program and regularly teaches classes on real-time kernels and other embedded software components.  Matt holds a bachelor's degree in computer engineering from Georgia Tech, Georgia in the USA.


  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Ram,

     

    The stack's ARP response should be automatic.  Anytime the stack needs an IP address for which it has no MAC address, it will send a request, and anytime that it receives a request for its own MAC address, it will provide a response.  Are you using one of the STM32 example projects from either the Micrium or element14 site?

     

    Regards,

     

    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks for your reply Matt,

     

     

    To get IP Packets we register a callback function(struct  net_if_api: Tx ) with TCP/IP Stack during initialization. In the same way , do we need to register any callback function 

    to get the ARP Packets or the same callback(currently receiving IP Packets) will be used by TCP/IP Stack to send the ARP Packets.

    I am not receiving any ARP Packets in the callback function (mentioned above) now.

    Is there any standard Micrium API which will be used by the TCP/IP Stack to send the ARP Packets.

     

    Thanks,

    Ram.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hi Matt,

     

    I'm running into an issue where one of the tasks encountered Hard Fault (which is one of interrupts that can't be disabled). At that point, nothing works anymore. If I were running a JTAG on the board, I can look at the OS Task Control Block and other parameters to determine which task was the culprit but as usual, issues don't always happen on the bench. So, how can I find out which task caused the problem? Is there a way for me to print out the task id? perhaps write to the flash memory?

     

    Any help is greatly appreciated!

    Thanks,

    Olaf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hey Matt,

    I am using MSP430 from TI . I am trying to send data through UART to PC from every task. However its not working. Transmit Buffer is loading with data but i am not able to receive data in my PC.

    Here is example of my code:

    i have called  the uart setup function in main function.

     

    void uart_setup()

    {

      OS_ERR err;

      OSSemPost(&MySem,OS_OPT_POST_1,&err);

      P3SEL = 0x30;                         

      UCA0CTL1 |= UCSWRST;           

      UCA0CTL1 |= UCSSEL_2;                     // SMCLK

      UCA0BR0 = 9;                              // 1MHz 115200 (see User's Guide)

      UCA0BR1 = 0;                              // 1MHz 115200

      UCA0MCTL |= UCBRS_1 + UCBRF_0;            // Modulation UCBRSx=1, UCBRFx=0

      UCA0CTL1 &= ~UCSWRST;                     // **Initialize USCI state machine**

      UCA0IE |= UCRXIE;                         // Enable USCI_A0 RX interrupt

    }

     

     

    void  AppTask1 (void *p_arg)

    {

        OS_ERR  err;

       while (1) {

           /

            send('1');

              OSTimeDlyHMSM(0u, 0u, 0u, 10u,

                          OS_OPT_TIME_HMSM_STRICT,

                          &err);

     

     

        }

    }

     

    // and my send function is like this:

    void send(char a)

    {

     

      while (!(UCA0IFG&UCTXIFG));             // USCI_A0 TX buffer ready?

        UCA0TXBUF = a;

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hey Matt,

    I am using Micrium OS 3 in MSP430 . I have made 10 Tasks in it. Is there any inbuilt function which can be used to directly jump from Task1 to suppose Task6 if all my Tasks are of same priority.

    Warm Regards,

    Krishna Kinger

     

     

    This thread has been closed to new questions.

    However, we welcome you to Post Your Question about Embedded in the element14 Community Embedded group. You'll find many fellow members and experts who have just the answer you're looking to find! 

     

    Thank You, Your Friends at element14 Community

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<