Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum New kid on the block - meet OLinuXino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 72 replies
  • Subscribers 503 subscribers
  • Views 6118 views
  • Users 0 members are here
  • sbc
  • single_board_computer
  • single_board_computers
  • low_cost
  • linux
Related

New kid on the block - meet OLinuXino

e14 Contributor
e14 Contributor over 14 years ago

Looks like certain berry-constant named device has opened Pandora's box, Olimex Ltd. just announced another low cost Linux SBC, but this time it is going to be OSHW and they are looking for developers that could help them round up the device for general use. Ok, enough talk, here's announcement - http://olimex.wordpress.com/2012/03/07/imx233-olinuxino-development-started-today/

 

PS read the article comments, this is not going to be the last OSHW SBC by Olimex image

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 14 years ago +1
    preliminary HW design at https://github.com/TsvetanUsunov/OLINUXINO Updates promised on Monday, looking ahead what comes out of it. Meant to be real open source hackerboard capable to run Linux and still…
  • e14 Contributor
    e14 Contributor over 14 years ago +1
    and now Yahoo group is open too http://tech.groups.yahoo.com/group/olinuxino
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini +1
    unfortunately those are Mbits and not MBytes (in MBytes that translates to 64MB) i.MX233 in LQFP package does not support more than that and chosen package is LQFP just so that design is replicatable by…
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hello World the embedded way, or Blinking LEDs:

    http://olimex.wordpress.com/2012/04/23/blinking-led-with-linux-or-hello-world-with-imx233-olinuxino/

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Hehe, I replied there.  I'm looking forward to that board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to morgaine

    It needs to be mentioned (just in case someone hasn't spotted it and is raising their expectations too high) that the OLinuXino that everyone is talking about, the one with Ethernet, is not going to be priced at 30 Euro at all, but at 45 Euro.  Olimex's price list is here:  http://www.olimex.com/dev/pricelist.html

     

    Summary:

    • iMX233-OLinuXino-Mini  - 29.95 Euro - 1 x USB only
    • iMX233-OLinuXino-Maxi - 44.95 Euro -  2 x USB + Ethernet

     

    The corresponding prices in US$ (since Raspberry Pi is quoted in US$) are US$39.31 and US$58.99 at today's exchange rate.  And for us Brits, that's UKP 24.42 and UKP 36.65 .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    at the same time it uses industrial grade components and should be usable in sub-zero (Celsius scale) temperatures.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    US$25 is a sort of "magic figure".  There's something about it that splits prices into two levels, those below it which frequently can be spent on a whim, and those above it which generally need careful consideration and budgeting.  Obviously the exact figure depends on personal finances, but typically it's around there somewhere.

     

    Raspberry Pi did a clever piece of marketting in promoting the Rpi as the "$25 computer" despite knowing full well that the vast majority of users would want the $35 version because a Linux machine without networking is pretty damn stupid in 2012.  Of course there are uses for a standalone Linux board, and the single USB on Rpi Model A could be used with a wifi dongle so the $25 version could still be "connected".  But nevertheless, the point stands that the $35 board is actually riding the marketting wave of the "$25 computer" headline.

     

    Olimex is obviously trying the same marketting "trick".  And it is genuinely a marketting trick, as they're advertising it as the "EUR 30 Linux Industrial grade single board computer", despite knowing that really it's the Ethernet version that could become really popular.  A person who isn't reading the blurb carefully might not catch the fact that there are two boards, and that the 30 Euro one doesn't have Ethernet.

     

    I like hardware, and I like the very capable hardware designers at Olimex and at the Raspberry Pi Foundation.  Marketing spin I don't like, and that applies to everyone, the Foundation included. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    US$25 is a sort of "magic figure".  There's something about it that splits prices into two levels, those below it which frequently can be spent on a whim, and those above it which generally need careful consideration and budgeting.  Obviously the exact figure depends on personal finances, but typically it's around there somewhere.

     

    Raspberry Pi did a clever piece of marketting in promoting the Rpi as the "$25 computer" despite knowing full well that the vast majority of users would want the $35 version because a Linux machine without networking is pretty damn stupid in 2012.  Of course there are uses for a standalone Linux board, and the single USB on Rpi Model A could be used with a wifi dongle so the $25 version could still be "connected".  But nevertheless, the point stands that the $35 board is actually riding the marketting wave of the "$25 computer" headline.

     

    Olimex is obviously trying the same marketting "trick".  And it is genuinely a marketting trick, as they're advertising it as the "EUR 30 Linux Industrial grade single board computer", despite knowing that really it's the Ethernet version that could become really popular.  A person who isn't reading the blurb carefully might not catch the fact that there are two boards, and that the 30 Euro one doesn't have Ethernet.

     

    I like hardware, and I like the very capable hardware designers at Olimex and at the Raspberry Pi Foundation.  Marketing spin I don't like, and that applies to everyone, the Foundation included. image