Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum New kid on the block - meet OLinuXino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 72 replies
  • Subscribers 503 subscribers
  • Views 6159 views
  • Users 0 members are here
  • sbc
  • single_board_computer
  • single_board_computers
  • low_cost
  • linux
Related

New kid on the block - meet OLinuXino

e14 Contributor
e14 Contributor over 14 years ago

Looks like certain berry-constant named device has opened Pandora's box, Olimex Ltd. just announced another low cost Linux SBC, but this time it is going to be OSHW and they are looking for developers that could help them round up the device for general use. Ok, enough talk, here's announcement - http://olimex.wordpress.com/2012/03/07/imx233-olinuxino-development-started-today/

 

PS read the article comments, this is not going to be the last OSHW SBC by Olimex image

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 14 years ago +1
    preliminary HW design at https://github.com/TsvetanUsunov/OLINUXINO Updates promised on Monday, looking ahead what comes out of it. Meant to be real open source hackerboard capable to run Linux and still…
  • e14 Contributor
    e14 Contributor over 14 years ago +1
    and now Yahoo group is open too http://tech.groups.yahoo.com/group/olinuxino
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini +1
    unfortunately those are Mbits and not MBytes (in MBytes that translates to 64MB) i.MX233 in LQFP package does not support more than that and chosen package is LQFP just so that design is replicatable by…
Parents
  • morgaine
    morgaine over 14 years ago

    Hooray, iMX233-OLinuXino is on Farnell's books at last! -- http://uk.farnell.com/olimex/imx233-olinuxino-maxi/sbc-linux-w-i-mx233-arm926j/dp/2144333?ref=lookahead .

     

    Not in stock yet, but at least the process has finally started, albeit one model only.  Still, it's progress. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago

    Hooray, iMX233-OLinuXino is on Farnell's books at last! -- http://uk.farnell.com/olimex/imx233-olinuxino-maxi/sbc-linux-w-i-mx233-arm926j/dp/2144333?ref=lookahead .

     

    Not in stock yet, but at least the process has finally started, albeit one model only.  Still, it's progress. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • fustini
    fustini over 14 years ago in reply to morgaine

    Groovy!  I'm happy to see more Open Source Hardware offered.  Hope it shows up on Newark, too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    I wonder if the forum threading problems have spread to the main web site.. It's apparently out of stock with 20 available for delivery:

    image

    Apart from that, I'm still having problems getting my head around something that's older tech, slower, and generally less capable than the Pi costing 14 quid more. Sure the Pi has it's issues, but with the amount of attention it has they're likely to get fixed sooner or later. Not yet convinced what future the OLinuxino has..

    The A13-olinuxino on the other hand.. if they can get the price below a BeagleBone and have them available here before the end of the year, that's a whole different story. Even then, the onboard, non usb, ethernet probably still ends up the better board image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Horses for courses.  Each device has its own area of application, and unless two devices are identical clones differing only in price, it's not reasonable to say that the higher priced one has no market.  It's likely to have some feature that the cheaper one lacks, and someone will want that feature.

     

    In the case of Raspberry Pi versus Olimex, I've not yet tested an OLinuXino, but I've tested a Pi and one thing is abundantly clear:  the Pi is very badly designed and some parts of it are completely broken, in particular the USB handling of RF mice on a self-powered hub.  I've never come across any kind of Linux board or computer with disastrously broken USB handling before, and it would be quite silly to expect the OLinuXino to be similarly broken or worse.

     

    Is a few pounds more worth paying for a product that works?  In my books that's a totally stupid question, because a non-working product is largely worthless.  I won't be buying any more Pi boards until such tier #1 problems are fixed, but I am certainly in the market for small and cheap Linux boards and therefore Olimex is of interest to me.

     

    On top of that, Olimex are responsive to problem reports and don't have a habit of banning you for insufficient praise.  That's worth a lot.  They are an engineering outfit, not a hype machine.  I like that.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 14 years ago in reply to morgaine

    Very true.

     

    You pick the processor or development board based upon your requirements.  Buying the cheapest is only valid if and only if it meets your requirements.

     

    All new devices are risky.  Until engineers have a chance to test it in a variety of applications, you will always have questions about its ability to meet your needs.

     

    So first define what you need, then look at the devices that meet all of your needs.  Then you can make a decision based upon capability and cost, but do not overlook the support tools that come with your choice.  You might save money on your device only to find you spend more time debugging your applications.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to DAB

    DAB wrote:

     

    ... but do not overlook the support tools that come with your choice.  You might save money on your device only to find you spend more time debugging your applications.

     

    A very good point.

     

    That is currently one of the problems with microcontroller work, because the most effective tools are proprietary and costly in their unrestricted versions, and this represents a hidden cost and liability for your project.  In contrast, open source tools remove that cost and the liability, but development efficiency can be reduced through less effective debugging or the hidden cost of having to roll your own.

     

    Finding the optimum solution is always a tradeoff, just like engineering a product always is, or just selecting one to buy.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 14 years ago in reply to morgaine

    Hi Morgaine,

     

    Yea that one has caused me a lot of grief in the past.

    It was the main reason that I finally had to agree with the company that standardizing on one line of MCU was more cost effective then letting each project just pick whatever was the new board available.  Without the proper tools, you just cannot do effective development, especially when you are doing one of a kind demonstration boards.

     

    It is a little better today with the open sources support, but when I started, we had little or nothing to work with.

    Plus you develope a better fell for both the devices and the tools as you reuse them on many projects.  It ends up giving you some of that extra time to include some bells and whistles.

     

    Just a thought,

    DAB