Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Altium and NXP collaborate to deliver component content online
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 502 subscribers
  • Views 210 views
  • Users 0 members are here
  • altium
  • altiumlive
  • embedded
  • Design
  • partnership
  • electronics
  • nxp
Related

Altium and NXP collaborate to deliver component content online

PRismaPR
PRismaPR over 14 years ago

image

 

 

Available in high resolution: info@prismapr.com

 

Altium and NXP collaborate to deliver component content online

New collection of NXP Semiconductors microcontroller component resources now available as design-ready content in AltiumLive

 

Shanghai, China – 9 May 2012 – Altium announces the release of a new range of board-level components for industry-leading ARMRegistered CortexTm-M3, CortexTm-M4 & CortexTm-M0 based microcontrollers from NXP Semiconductors to their subscription customers through AltiumLive.

Designing with components for NXP’s LPC1800 microcontrollers based on Cortex-M3 provides users with high performance operating speeds of up to 180 MHz, large on-chip memories, high-speed USB, SPI Flash Interface, and State Configurable Timers whilst the LPC1100 microcontrollers based on Cortex-M0 gives you instant access to low-cost, easy to use and energy-efficient processors.

Also available to Altium users, are the high-performance, low-cost, digital signal processing capabilities which are introduced with the new Digital Signal Control (DSC) processors for the LPC4300 microcontroller series based on the Cortex-M4. “Collaboration with NXP has enabled us to provide easy access to the Cortex-M3, Cortex-M4 & Cortex-M0 based microcontrollers for our global Subscription customers.” said Rowland Washington, Content Development Manager for Altium. “This update is delivered as part of our content-driven subscription model and further expands on our range of third-party, design-ready IP for our customers.”

Relationships with electronics suppliers such as Digi-Key, Mouser and Newark allow us to provide the Altium community with board-level components that include real-time supply-chain information, such as supplier choice, pricing and availability. With this release, electronic designers now have access to a set of new, supply-chain enabled devices which will complete the Cortex-M3, Cortex-M4 and Cortex-M0 board-level component support available in AltiumLive. The collection from NXP Semiconductors can be seen in the Unified Components store.

“Collaborating with Altium to deliver high-quality component models through AltiumLive will enable design engineers to harness the benefit of NXP microcontrollers with Altium's extensive design library.” said Ken Dwyer, Applications Engineering Manager, NXP Semiconductors. “With these components now easily available, it will save hardware engineers valuable time and also speed up the design cycle.” This component release joins the numerous content updates released through the AltiumLive platform to provide Altium Subscription customers with the latest design content available. More information on the board-level components and how they are accessed in Altium Designer is available from AltiumLive and in the related blogs. NXP products are available directly from NXP online or from a range of NXP authorized distributors worldwide. For more information, go to http://www.nxp.com/microcontrollers.

ENDS

Contact:

Frank Krämer

Altium Europe GmbH

+49 721 8244 108

frank.kraemer@altium.com

 

Gabriele Amelunxen

PRismaPR +49 8106 247 233

info@prismapr.com

 

Monika Cunnington

PRismaPR (UK)

+44 1462 640 779

monika@prismapr.com

www.prismapr.com

 

About Altium

Altium Limited (ASX:ALU) creates electronics design software and services based on the belief that anyone who wants to create electronic products that make a difference should be able to do so. Altium’s unified electronics design environment links all aspects of electronics product design in a single application that is priced to be as affordable as possible. This allows electronics designers break down barriers to innovation, harness the latest devices and technologies, manage their projects across broad design ecosystems, and create connected, intelligent designs.

Founded in 1985, Altium has headquarters in Shanghai, and operates worldwide. For more information, visit www.altium.com. You can also follow and engage with Altium via Facebook, Twitter and YouTube.

 

About NXP Semiconductor Products

NXP Semiconductors N.V. (NASDAQ: NXPI) provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power Management, Interface, Security and Digital Processing expertise. These innovations are used in a wide range of automotive, identification, wireless infrastructure, lighting, industrial, mobile, consumer and computing applications. A global semiconductor company with operations in more than 25 countries, NXP posted revenue of $4.2 billion in 2011. For more information, visit www.nxp.com.