Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Altium instrumental in breaking down the barrier to commercial space travel
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 502 subscribers
  • Views 247 views
  • Users 0 members are here
  • altium
  • designer
  • space
  • Design
  • Technology
  • spacex
  • electronics
  • dragon
Related

Altium instrumental in breaking down the barrier to commercial space travel

PRismaPR
PRismaPR over 14 years ago

image

 

SpaceX designs electronics for world’s first successful private space flight with Altium Designer’s unified development tool

 

Space transport start-up Space Exploration Technologies, or SpaceX, made history last month when its Dragon spacecraft returned to Earth following the first successful mission by a private company to carry supplies to the International Space Station. The Altium Designer unified development environment helped SpaceX develop electronic circuitry that meets the high levels of quality and reliability demanded from space technology at a commercially viable cost.

 

Space has long been a field reserved for big spenders such as governments and large companies. However with rapid advances in electronics and information technology, SpaceX has managed to break through the cost barrier with its family of low-cost Falcon launch vehicles and the Dragon spacecraft. 

 

To ensure its launch vehicles always meet the highest level of quality and reliability, SpaceX develops many of its boards and controllers in-house under the fault–tolerant discipline. This complex and time consuming engineering technique ensures that all systems can continue to operate despite a given component failing.

 

SpaceX found that by incorporating Altium Designer into its production process, the design process could be simplified considerably. Thanks to Altium’s enhanced version control features, SpaceX was able to better manage its ongoing design development. Altium’s live design capabilities meant that the simplest modifications could be automatically adjusted in all previous board and schematic work. The result was a flexible, reliable and cost-effective development and documentation process for SpaceX’s catalogue of PCB designs.

 

Altium’s comprehensive libraries were found to be one of the biggest development boons for SpaceX. The library feature provided engineers with the latest and most up-to-date components in a user-friendly system. Engineers were also able to add new components, which allowed for greater customization and board enhancements.

In addition, design flows were complemented by Altium Designer’s ready-to-use FPGA-based components for instant FPGA integration. This feature meant SpaceX could immediately employ FPGAs into its designs, easily capturing them at the schematic level. With the features combined, SpaceX had a complete set of solutions in a single platform system.

 

SpaceX found that by using Altium Designer, it could build avionic systems that meet the same quality standards as those used in multi-million dollar satellite projects at a much lower cost. This was confirmed by the successful launch of the Dragon spacecraft which reached the space station at its first attempt, transferred its cargo without problem and then safely returned to Earth. The electronics designed with Altium played a crucial part in this success.

 

 

ENDS

 

Contacts:

Frank Krämer
Altium Europe GmbH
+49 721 8244 108
frank.kraemer@altium.com

 

Gabriele Amelunxen
PRismaPR
+49 8106 247 233
info@prismapr.com

 

Monika Cunnington
PRismaPR (UK)
+44-1462 640 779
monika@prismapr.com

 

www.prismapr.com

 

 

About Altium

Altium Limited (ASX:ALU) creates electronics design software based on the belief that anyone who wants to create electronic products that make a difference should be able to do so. Altium’s unified electronics design environment links all aspects of electronics product design in a single application that is priced to be as affordable as possible. This helps electronics designers break down barriers to innovation, harness the latest devices and technologies, manage their projects across broad design ‘ecosystems’, and create connected, intelligent designs.

 

Founded in 1985, Altium has headquarters in Shanghai, and operates worldwide. For more information, visit www.altium.com. You can also follow and engage with Altium via Facebook, Twitter and YouTube.

 

Altium, Altium Designer, AltiumLive and Morfik, and their respective logos, are trademarks or registered trademarks of Altium Limited, or its subsidiaries. All other registered or unregistered trademarks mentioned in this release are the property of their respective owners, and no trademark rights to the same are claimed.

 

June 20, 2012