Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Altium releases new TASKING C compilers for Power Architecture and RH850, targeting ISO 26262 application development
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 502 subscribers
  • Views 279 views
  • Users 0 members are here
  • altium
  • designer
  • freescale
  • 26262
  • Technology
  • viper
  • iso
  • stmicroelectronics
  • tasking
Related

Altium releases new TASKING C compilers for Power Architecture and RH850, targeting ISO 26262 application development

PRismaPR
PRismaPR over 13 years ago

image

Harm-André Verhoef,

Product Manager for TASKING at Altium

Image available: info@prismapr.com

 

Altium releases new TASKING C compilers for Power Architecture and RH850, targeting ISO 26262 application development

 

Karlsruhe, Germany, 16 October 2012 – Altium has released two completely new TASKING C compiler solutions for automotive application development, delivering support for the RH850 microcontrollers from Renesas and the Power ArchitectureRegistered based microcontrollers from the Freescale Qorivva/5xxx and STMicroelectronics SPC56 series. These new development solutions extend the range of popular TASKING toolsets for automotive microcontrollers like XC2000, ARM, ST10 and TriCore.

Both new compilers have been developed from the ground up, using Altium’s highly efficient Viper “VX” compiler technology, not limited by legacy compiler implementations. This new generation of compilers is the perfect clean start towards ISO 26262:2011 certified development tools and application development.

Viper is a modern compiler technology fully developed and owned by Altium and as such does not depend on components from third parties or the public domain. The use of Viper technology guarantees compatibility to other popular TASKING toolsets which have established a solid “proven in use” reputation with highly efficient and robust code for automotive applications like power train, body control, chassis control and safety critical applications.

"Internal and external automotive application benchmarks with the new C compilers have shown best-in-class code efficiency achievements," says Harm-André Verhoef, Product Manager for TASKING at Altium. "This is a clear result of our close cooperation with customers and the understanding of their code optimization needs and we are very proud of our leading position here. The new compilers excel in build-time efficiency, delivering significant product development time and cost savings to developers."

The TASKING Viper technology features MISRA C and CERT C code checking, profiling through code instrumentation and run-time error checking capabilities. Using Viper technology programmers can now develop extremely robust code in significantly less time than previously possible.

The new compilers are available immediately for evaluation and use by automotive OEMs and Tier 1s. ISO 26262 compliance and certification will be completed in 2013. Addressing the needs of broad and emerging markets, an IDE and debugger will be added to the compilers, delivering a cost-effective complete solution to developers.

All licensed users will be updated with an ISO 26262 certified compiler and IDE/debugger on availability. Altium’s regular annual service agreements, legacy service models and long-term service models are available to back up the new products with technical support and Altium's commitment to support new family members of the respective microcontrollers.

 

ENDS

Contacts:

Frank Krämer

Altium Europe GmbH

+49 721 8244 108

frank.kraemer@altium.com

 

Gabriele Amelunxen

PRismaPR

+49 8106 247 233

info@prismapr.com

 

Monika Cunnington

PRismaPR (UK, Scandinavia & Benelux)

+44 20 8133 6148

monika@prismapr.com

www.prismapr.com

 

About TASKING

TASKING development tools are used by carmakers and the world's largest automotive Tier 1 suppliers to program microcontroller-based power train, body control and safety-related applications worldwide. More than 10.000 users rely on TASKING compilers and debuggers to create richer next-generation applications while achieving optimum reliability, security, and performance. TASKING compilers are also part of Altium Designer and installed on hundreds thousands of developers’ desktops around the globe. In 2012 the TASKING brand celebrates 35 years of technology leadership, quality tools and customer support excellence.

About Altium

Altium Limited (ASX:ALU) creates electronics design software based on the belief that anyone who wants to create electronic products that make a difference should be able to do so. Altium’s unified electronics design environment links all aspects of electronics product design in a single application that is priced to be as affordable as possible. This helps electronics designers break down barriers to innovation, harness the latest devices and technologies, manage their projects across broad design ‘ecosystems’, and create connected, intelligent designs.

Founded in 1985, Altium has headquarters in Shanghai, and operates worldwide. For more information, visit www.altium.com. You can also follow and engage with Altium via Facebook, Twitter and YouTube.

Altium, Altium Designer, AltiumLive and their respective logos, are trademarks or registered trademarks of Altium Limited, or its subsidiaries. All other registered or unregistered trademarks mentioned in this release are the property of their respective owners, and no trademark rights to the same are claimed.