Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Altium Designer update integrates new functionality based on customer feedback
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 502 subscribers
  • Views 202 views
  • Users 0 members are here
Related

Altium Designer update integrates new functionality based on customer feedback

PRismaPR
PRismaPR over 13 years ago

Visit Altium at electronica 13 – 16 November 2012, Hall A1, Stand 659

Text and picture available: http://go.altium.com/press-electronica.html

 

Press Release 18/2012

 

Altium Designer update integrates new functionality based on customer feedback

 

Latest updates for Altium Designer platform now available for Altium Subscription customers through continuous update model

 

electronica, Munich – 13 November 2012 – Altium, developer of next generation electronics design software and services, announced the 22nd update for Altium Designer since the release of Altium Designer 10 in March 2011.

 

This update delivers additional enhancements to Altium Designer as well as specific improvements and new functionality based on Altium Subscription customer feedback. It includes updated FPGA device and vendor tools support for Xilinx ISE 14.2 and Lattice Diamond 2.0 plus a new module for IDF export. The latter can be used in the batch process of OutJobs to create IDF data automatically during the release process together with all other information needed for documentation or production.

 

Incremental Unroute

During the interactive routing of the PCB and especially while re-using existing boards, unrouting existing tracks is a common task on the way to get best results. With this update, Altium implements a smart way to unroute existing tracks using an incremental process to delete selected routing objects with automatic selection of the adjacent routing objects. Users can easily repeat this process to come to the desired result while saving time compared to the previous implementation.

 

To deliver these key new features to the users, the continuous update model from Altium is used. This allows Altium to provide new features and enhancements as soon as they are ready without the need to wait for the next service pack or major update.

 

Availability

The latest update for Altium Designer is available for Altium Subscription customers as part of their subscription benefits at no extra cost. The update can be accessed and installed very easily through Altium Designer and its 'Plug-ins and Updates' page (DXP >> Plug-ins and updates). Designers without Altium Subscription should contact their local Altium Sales & Support Centre or Reseller for advice on the available options and how to get up to date again.

 

ENDS

 

Contacts:

Frank Krämer

Altium Europe GmbH

+49 721 8244 108

frank.kraemer@altium.com

 

Gabriele Amelunxen

PRismaPR

+49 8106 247 233

info@prismapr.com

 

Monika Cunnington

PRismaPR (UK, Skandinavia, Benelux)

+44-20 8133 6148

monika@prismapr.com

www.prismapr.com

 

About Altium

Altium Limited (ASX:ALU) creates electronics design software based on the belief that anyone who wants to create electronic products that make a difference should be able to do so. Altium’s unified electronics design environment links all aspects of electronics product design in a single application that is priced to be as affordable as possible. This helps electronics designers break down barriers to innovation, harness the latest devices and technologies, manage their projects across broad design ecosystems, and create connected, intelligent designs.

Founded in 1985, Altium has headquarters in in Shanghai, and operates worldwide. For more information, visit www.altium.com. You can also follow and engage with Altium via Facebook, Twitter and YouTube.