Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Qseven Tablet PC Demonstration Platform Heralds New Age of Flexible Design
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 502 subscribers
  • Views 186 views
  • Users 0 members are here
  • c-pad
  • pc
  • coms
  • congatec
  • platform
  • computer-on-modules
  • demonstration
  • tablet
Related

Qseven Tablet PC Demonstration Platform Heralds New Age of Flexible Design

PRismaPR
PRismaPR over 13 years ago

Reader Enquiries:

congatec AG

Christian Eder

Phone: +49-991-2700-0

info@congatec.com

www.congatec.com

 

Press Contact:

PRismaPR (UK, Scandinavia + Benelux)

Monika Cunnington

Phone: +44-20-8133 6148

monika@prismapr.com

www.prismapr.com

 

PRismaPR

Bettina Lerchenmüller

Phone: +49-8106-24 72 33

info@prismapr.com

www.prismapr.com

 

Visit congatec at embedded world 26 – 28 February 2013 Hall 1, Stand 350

 

image

Text and photograph available: http://www.congatec.com/press

Video available: www.youtube.com/watch?v=Wc3l82UwJH8

 

Press release 03/2013

 

Qseven Tablet PC Demonstration Platform Heralds New Age of Flexible Design

 

The Latest High-Performance, Low-Power Computer-On-Modules Enable Simpler, Faster and More Flexible Designs

 

embedded world, Nuremberg, 26 February 2013  * * *  congatec AG, a leading manufacturer of embedded computer modules, is demonstrating a Tablet PC Technology Demonstration Platform targeting industrial applications at embedded world 2013, Hall 1, Stand 350. T

his Qseven Pad Demonstration Platform vividly illustrates the flexibility of modular programming and its ability to drastically reduce the design time and complexity of compact equipment, such as an industrial Tablet PC.

It’s based on congatec’s class-leading Qseven module conga-QMX6, which features Freescale’s latest i.MX6 processor, providing scalability from a single- to a dual- and even quad-core processor in the same low-power high-performance form factor. Using ARM’s state-of-the-art Cortex-A9 processor, with fully integrated graphics acceleration, enables the conga-QMX6 to deliver the low power and high performance needed in highly demanding applications and portable devices such as a ruggedized Tablet PC. As many Tablet PCs are now based on ARM’s Cortex-A9, a Tablet PC featuring a conga-QMX6 would have exactly the same performance as a full-custom design using the same, or similar, processor but with significantly less design cost and complexity.  The congatec pad demonstrator also utilizes congatec’s SBM3 SMART Battery Manager Module to manage the complete power conversion, distribution and monitoring. The Demonstration Platform runs an embedded Linux version. However, this Platform is also capable of running other operating systems such as Android or Microsoft Windows Embedded Compact 7 (WEC7).

congatec’s R&D Manager, Carsten Rebmann, commented: “This demonstration platform is intended to show how the flexibility and scalability of modular computing can be quickly and easily configured to target applications with even the most demanding requirements.” Most Tablet PCs are still commonly developed using a full-custom approach, which introduces unnecessary complexity. The Demonstration Platform uses standard components; further adaptations can be implemented easily by creating a customer-specific carrier board. The standard carrier board can be used as a perfect base to add specific functionalities. Customized tablet computers can be created fast and with less design risk.

Tablet PCs are increasingly common in the industrial sector and are used to provide remote HMIs (Human-Machine Interfaces) as well as local control. Industrial installations often span large distances; with a Tablet PC operators are able to take the control interface with them as they operate the machine.

The congatec Tablet Demonstration Platform is on display at congatec’s stand at embedded world 2013 in Hall 1 Stand 350. 

 

About congatec

AG congatec AG has its head office in Deggendorf, Germany and is a leading supplier of industrial computer modules using the standard form factors Qseven, COM Express, XTX and ETX. congatec’s products can be used in a variety of industries and applications, such as industrial automation, medical technology, automotive supplies, aerospace and transportation. Core knowledge and technical know-how includes unique extended BIOS features as well as comprehensive driver and board support packages. Following the design-in phase, customers are given support via extensive product lifecycle management. The company’s products are manufactured by specialist service providers in accordance with modern quality standards. congatec currently has 135 employees and entities in Taiwan, Japan, USA, Australia and the Czech Republic. More information is available on our website at www.congatec.com or via Facebook, Twitter and YouTube. Copyright 2013 congatec AG