Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Altium Designer 2013 Available
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 502 subscribers
  • Views 284 views
  • Users 0 members are here
  • altium
  • designer
  • 2013
  • tasking
Related

Altium Designer 2013 Available

PRismaPR
PRismaPR over 13 years ago

image

  Image available: info@prismapr.com

 

Visit Altium at embedded world 26 – 28 February 2013, Stand 5-445 for Altium Designer Stand 4-618 for TASKING

 

Press Release 02/2013

 

Altium Designer 2013 Available

 

A Paradigm Shift - Altium Re-engineers and Opens Up its DXP Platform

 

Shanghai, China – 7 February 2013 – Altium Ltd., a global leader in Smart System Design Automation and provider of solutions for 3D PCB design (Altium Designer) and embedded software development (TASKING), announces the release of Altium Designer 2013.

This is a significant turning point in Altium’s history, as Altium Designer 2013 not only delivers new and enhanced features, it also opens up Altium’s design platform to key partners. This creates a range of opportunities for users, partners and system integrators and represents a quantum leap for the industry.

As part of Altium’s continuous content delivery model, Altium Subscription customers have already benefited from the many enhancements that have been delivered since Release 12. Altium Designer 2013 further improves the design environment for users by delivering several new PCB features and updates to the core PCB and Schematic tools.

 

Key new features of Altium Designer 2013 include:

• Addition of PCB object and Layer transparency settings to the View Configurations dialog.

• Silk to Solder Mask design rule with new checking modes (to exposed copper and to solder mask openings).

• Outline vertices editor for PCB Polygon Pours, Polygon Cutouts and Solid Region objects.

• Ability to define polygonal-shaped blanket directives.

• Schematic Pin name/designator position, font and color customization.

• Individual port height and font control.

• Text objects in schematic documents now support hyperlinks.

• Smart PDF documents contain component parameters - Clicking on a component in a PDF file produced by SmartPDF will display the parameters of that component.

• Support for Microchip mTouch capacitive controls.

• Upgraded DXP platform to provide a robust and open development environment.

 

A full overview of Altium Designer 2013 can be found in the Altium Wiki.

In addition, Altium’s new AppsBuilder will be available shortly, which will allow for the creation of custom applications and extend Altium’s DXP design environment even further.

“The release process for Altium Designer 2013 was one of the most intense we have been through to date but the interaction and collaboration with some of our most engaged customers made it one of the most successful,” says Matt Schwaiger, a senior member of Altium’s Product Management team. “It’s the collaboration with our users which ensures features and enhancements delivered bring the most value to our community as a whole.”

 

Frank Hoschar, CMO at Altium says: “Altium Designer 2013 is a milestone release as it provides an open platform expanding Altium’s reach beyond our user community (of more than 80,000 engineers working on the DXP platform) into industry partner communities. Additionally, Altium Designer provides a number of key enhancements from Altium Designer 12, which include new

• Via Stitching capabilities providing support for RF and high-speed designs,

• Greater flexibility for re-annotating PCB designs,

• Other PCB productivity enhancements including improved cross-select mode, improved selection controls and easier polygon pour management

• Improvements to the Mentor PADS PCB, PADS Logic and Expedition importers as well as Ansoft and Hyperlynx exporters,

• Support for ARM Cortex-M3 Discrete Processors, SEGGER J-Link and Altera Arria2GX FPGAs.”

 

License options

Altium Designer 2013 is available with the following license options:

 

• Altium Designer 2013 This license provides users with full custom board design and manufacturing capabilities. It also has complete front-end engineering design and verification system for both board-level and programmable logic design and full 3D PCB design and editing capabilities.

• Altium Designer 2013 SE This is the System Engineering version that provides users with complete front-end schematic design and design capture for both board-level and programmable logic design. It includes analog/digital simulation, verification and Embedded-System-on-FPGA implementation.

 

Pricing and availability Altium Designer 2013 is available immediately for Altium Subscription customers as part of their subscription. Eligible customers can download the new Altium Designer 2013 installer from AltiumLive. The price for a perpetual licence of Altium Designer 2013 is 5.395 EUR incl. 1-year subscription (updates, support, additional content and services), Altium Designer 2013 SE is available for 2.215 EUR incl. 1-year subscription.

 

ENDS

 

Contacts:

Frank Krämer

Altium Europe GmbH

+49 721 8244 108

frank.kraemer@altium.com

 

Gabriele Amelunxen

PRismaPR

+49 8106 247 233

info@prismapr.com

 

Monika Cunnington

PRismaPR (UK, Scandinavia, Benelux)

+44-20 8133 6148

monika@prismapr.com

www.prismapr.com

 

About Altium

Altium Limited (ASX:ALU) creates electronics design software. Altium’s unified electronics design environment links all aspects of electronics product design in a single application that is priced as affordable as possible. This enables electronics designers to innovate, harness the latest devices and technologies, manage their projects across broad design ‘ecosystems’, and create connected, intelligent designs. Founded in 1985, Altium has headquarters in Shanghai, and operates worldwide. For more information, visit www.altium.com. You can also follow and engage with Altium via Facebook, Twitter and YouTube.