Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum MPLAB X v1.70 disponible pour Linux, MAC OS et Windows
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 502 subscribers
  • Views 284 views
  • Users 0 members are here
  • ide
  • microchip
  • mplabx
  • pic24
  • dspic33
  • mplab
  • microcontroleur
  • microcontroller
  • dspic
  • pic32
  • pic
Related

MPLAB X v1.70 disponible pour Linux, MAC OS et Windows

MicrochipRTCfr
MicrochipRTCfr over 13 years ago

image

La version v1.70 est désormais disponible en téléchargement ici : http://www.microchip.com/mplab

 

MPLAB  X est disponible sous Linux, MAC OS et Windows ainsi que les  compilateurs (XC8, XC16 et XC32) dont il existe des versions gratuites téléchargeables ici :  http://www.microchip.com/compilers

 

Release notes :

 

  • Makefile Projects – Allows you to build outside the IDE via the command line, i.e., no management of the makefile or build process within the IDE. Also, you can choose the artifact of the build that you want to load into IDE memory once the build is complete.
  • PIC32 SKDE connection stabilization – Resolved several connection issues.
  • HCS device programming support added for PICkit 3, MPLAB ICD 3, and MPLAB REAL ICE in-circuit emulator – You may now program Secure Devices (HCS) with these tools.
  • Graphical Display Designer (GDD) for MPLAB X IDE v1.00 available – This plug-in from MPLAB IDE v8 is now available in MPLAB X IDE.
  • MPLAB IPE Engineering mode - Allows the engineer to set parameters that can and cannot be adjusted by a technician. 

 

Des formations MPLAB X (TLS0101 et TLS0999) sont proposées tous les mois dans les centres de formations Microchip (Paris, Milan, Münich, USA,...)

Planning des formations et inscription sur internet : http://www.microchip.COM/RTC

 

Catalogue des formations ci-joint

Attachments:
imageMicrochip_catalogue_formations_WEB_Q3B_2012_120906.pdf