Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Best choice for camera interface
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 502 subscribers
  • Views 1111 views
  • Users 0 members are here
  • cameras
  • embedded
  • ptz
Related

Best choice for camera interface

e14 Contributor
e14 Contributor over 11 years ago

Hi there,

I am going to design a smart surveillance system in which I will be using PTZ cameras with a controller kit. I need some guidance about the choice of processor to be used. Size of the board is not a figure of merit.
Regards.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago +1
    Hello abubaker , Assuming you have great PTZ camera's with reasonable till high resolutions then Arduino won't be able to process the video stream and detect motion because it is far too light. As a learning…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor +1
    abubaker Fortunately ZM is open source and ZM's "zone minding" can be controlled. someone hacked that already ZoneMinder - Wiki - How to control your Foscam HD cameras - PTZ cheers, Fred
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hello abubaker ,

     

    Assuming you have great PTZ camera's  with reasonable till high resolutions then

    Arduino won't be able to process the video stream and detect motion because it is far too light.

     

    As a learning process I would suggest to hack one of those cheap Chinese camera' s like in this instructable. http://m.instructables.com/id/Hack-a-30-WiFi-Pan-Tilt-Camera-Video-Audio-and-Mot/

    However unlike this instructable that only catches and processes the available streams, completely replace the internal weak embedded system with FramboisePie 2 ;)

    The original code of those camera's is available somewhere as I remember from a few years ago.

    The maximum resolution of such camera is limited at 640x480 pixels.

    This type of camera at its minimum 5 till max 30 fps can hardly cope with that bunch of data and will normally crash and reboot itself sometimes. Clearly a trade off was done for the processing power and internal memory. Positive side of these things is that they have speaker and mic build-in and can see in the dark quite ok assisted by the build-in IR leds.

    In the hacking process also suggest to introduce some kind of vpn tunnel with ssl or something because these camera's are basically quite open to the internet.

     

    good luck with your project!

     

    cheers,

    Fred

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    abubaker,

    Of course zoneminder comes to mind ;)

    See someone did it already on previous version of Framboise Pie ;)

    http://www.holylinux.net/content/raspberry-pi-webcam-zoneminder

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Zone minder is typically for CCTVs not for PTZs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    abubaker


    Fortunately ZM is open source and ZM's "zone minding" can be controlled.

    someone hacked that already image

    ZoneMinder - Wiki - How to control your Foscam HD cameras - PTZ

     

    cheers,

    Fred

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    abubaker


    Fortunately ZM is open source and ZM's "zone minding" can be controlled.

    someone hacked that already image

    ZoneMinder - Wiki - How to control your Foscam HD cameras - PTZ

     

    cheers,

    Fred

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    thanks Fred..