Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Technical trainings : introduction to embedded C language for control engineers (feb 4th & 5th 2014)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 502 subscribers
  • Views 196 views
  • Users 0 members are here
  • microchip
Related

Technical trainings : introduction to embedded C language for control engineers (feb 4th & 5th 2014)

MicrochipRTCfr
MicrochipRTCfr over 12 years ago

image

 

Dear Customer,

 

Based on numerous customer requests, Microchip Technology is happy to announce the next set of Technical trainings which will take place in its UK based training center in Winnersh.

 

Subjects will cover :

·         Introduction to the C Programming language for embedded engineers

·         A 2 days cursus around the low-cost 8 bits PIC10/12/16 microcontroller families

 

Dates : 4th to 7th of february 2014

Location : Microchip Technology (Winnersh)

 

Technical trainings : Embedded C, MPLAB X, 8 bits MCUs (PIC10/12/16)

(Introduction to Embeddedd C + MPLAB X + 8 bits Architecture + Peripherals) [4 Days]

 

DESCRIPTION AND PRE-REQUISITES :

 

Training Reference

Description

Duration

/ Price (excl.VAT)

Pre-requisites

TLS 2101 (4+5/2/2014)

Introduction to the C Programming Language for Embedded Control Engineers

2 days

(400 GBP)

Basic microprocessor / microcontroller  know-how

TLS 0101

(6/2/2014 AM)

Getting Started with Microchip Development Tools (MPLAB X)

½ day

(60 GBP)

Basic microprocessor / microcontroller  know-how

MCU 1101

(6/2/2014 PM)

Getting Started with Microchip's 8-bit MCU Architecture and Instruction Set

½ day

(60 GBP)

Level 1 / Hands-on labs

MPLAB X usage, basic C knowledge. Classes TLS 0101 recommended beforehand

MCU 1121

(7/2/2014)

Microchip Mid-Range PICRegistered MCU Peripherals

 

1 day

(120 GBP)

Level 2 / Hands-on labs

MPLAB X usage, basic C knowledge. Classes TLS 0101 &  MCU 1101 recommended beforehand

 

NOTES : several hands-on labs are realized during each session.

              Each participant has its own dedicated equipment (laptop PC + development tools).

              The course material, exercises and their solutions (source code) will be provided to each participant 

              on a CD-ROM.

 

 

Class Reference TLS 2101 ( 2 days) :

 

Introduction to the C Programming Language for Embedded Control Engineers

 

This 2 days class provides an introduction to the C programming language (as specified by the ANSI C89 standard) in the context of embedded systems.

We will cover the C language from the ground up from a non-hardware specific point of view in order to focus on the various elements of the C language itself.

 

While not required, previous experience with any programming language or experience with microcontrollers would be helpful.

 

The presentation will be accompanied by a series of hands-on exercises designed to reinforce the fundamentals, all of which will be conducted within MPLAB X using the 16 bit C compiler and Simulator.

Skills learned in this class will be applicable to any ANSI C compiler.

 

Hardware and compiler specific details such as interrupts, memory models and optimization will NOT be discussed. These topics will be covered in the compiler specific classes.

 

 

 

 

 

Class Reference TLS 0101 ( ½ day ) :

 

Getting Started with Microchip Development Tools (MPLAB X)

 

This class provides an introduction to Microchip development tools. Following an introduction to all Microchip tools, hands-on exercises are conducted using the MPLAB X IDE, the MPLABRegistered SIM simulator and the MPLAB-ICD3 or REAL ICETm. Attendees go through a step-by-step creation of a project, editing and compiling a program, running a program and using the simulator. The debugger is then used to connect the microcontroller to the PC hardware in order to program an actual device and run a program. Debug capabilities are introduced and debugging basics are described – how to set a breakpoint, etc. Debugging will be performed either with Proteus simulator plugin or with hardware tools (ICD3, Real-Ice & the Explorer-16 demoboard)

 

 

 

 

 

Class Reference : MCU 1101  ( ½ day ) :

Getting Started with Mid-Range Microcontroller Family Architecture and Instruction Set

This class covers the fundamentals of the Mid-Range microcontroller family’s architecture and instruction set. Topics covered include the programmer’s model, data and program memory organization, clocking structures, assembly language and special features of the devices. Basic concepts are reinforced through the writing of simple C / assembly language programs. This process involves the use of the simulator to simulate and debug the programs. Ultimately, a PIC16 microcontroller is programmed using the MPLABRegistered ICD 3 on a PICDEMTm 2 Plus demonstration board.

 

 

 

Class Reference : MCU 1121 ( 1 day ) :

Microchip Mid-Range PICRegistered MCU Peripherals

This class covers the configuration and usage of the Mid-Range microcontroller family peripherals including timers, A/D converters, UARTs, comparators, PWMs and more. Interrupt structures and interrupt service routine handling are also covered. Attendees go through multiple hands-on exercises and learn how to program Mid-Range devices. Labs are offered in C or assembly

 

.

 

    Attendees will get a 20% discount coupon valid on all Microchip tools (HW & SW)

 

 

 

 

 

Training Location :

 

Microchip House

 

720 Wharfedale Road

 

IQ Winnersh

 

Wokingham, Berkshire

 

RG41 5TP UK

 

 

 

Registrations : http://www.microchip.com/RTC

 

 

 

More Informations ?

 

Microchip Technology UK :  01189 215800

 

eMail : formation at microchip dot com

 

 

 

Attachments:
Training_C+8B_MX+PIC16_www_4D_131218.pdf