Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Modbus
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 503 subscribers
  • Views 548 views
  • Users 0 members are here
  • modbus
Related

Modbus

e14 Contributor
e14 Contributor over 12 years ago

Does modbus use to communicate between sensor and data acquisition system?

  • Sign in to reply
  • Cancel
Parents
  • sqkybeaver
    sqkybeaver over 12 years ago

    modbus is primarily used in industrial control and automation. developed by Modicon(Schneider Electric) it is a protocol using rs-232, rs-485 or Ethernet, it is a packet based communications standard. common devices that use modbus include(not limited to) PID controllers, programmable logic controllers, motor controllers, and user interface systems.

     

    the serial based protocol can be fairly easy(compared to Ethernet) to implement into a small microcontroller system using standard uart.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • sqkybeaver
    sqkybeaver over 12 years ago

    modbus is primarily used in industrial control and automation. developed by Modicon(Schneider Electric) it is a protocol using rs-232, rs-485 or Ethernet, it is a packet based communications standard. common devices that use modbus include(not limited to) PID controllers, programmable logic controllers, motor controllers, and user interface systems.

     

    the serial based protocol can be fairly easy(compared to Ethernet) to implement into a small microcontroller system using standard uart.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to sqkybeaver

    Thank you for this information. So you means that modbus is a packet based communication protocol.

    1> So that means on both side (master and slave) microcontroller must be there to process the request or to give the         response.

    2> Sensor doesn't have any microcontroller means if sensor is equipped with microcontroller circuit then only data acquisition system and sensor communication over modbus protocol is possible.

    Is these both points are correct or not ? If not then please correct me.