Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Where do I start  in embedded?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 37 replies
  • Subscribers 504 subscribers
  • Views 4094 views
  • Users 0 members are here
  • microcontrollers
  • embedded
Related

Where do I start  in embedded?

majorkuso
majorkuso over 11 years ago

I would like to get better at building embedded devices but can't decide between avr or pic. I have the pickit 3 for pics and avr usbasp  and arduino. the arduino is ok, but I want to get closer to the metal. I would like some structured projects that I can build and familiarize myself with both the hardware and more importantly the c coding i would like to get better at my c. What would you guys recommend?

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 11 years ago in reply to dougw +2
    Caveat: PSoC4 and PSoC5 are great chips, but the PSoC Creator environment you need to design with them only runs on Microsoft Windows.
  • DAB
    DAB over 11 years ago +1
    Hi James, I would suggest the cypress Semiconductor PSOC 4 family. They have a great free development IDE plus they have programmable hardware for digital and analog circuits. They have a great range of…
  • Jan Cumps
    Jan Cumps over 11 years ago +1
    You can go to the very metal with that Arduino that you have. There's no need to invest.
Parents
  • Jan Cumps
    0 Jan Cumps over 11 years ago

    You can go to the very metal with that Arduino that you have. There's no need to invest.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • majorkuso
    0 majorkuso over 11 years ago in reply to Jan Cumps

    I would like to take the arduino out of the equation if possible. that way I could get the clock speed of the avr or pic just trying to find a good set of courses or something that can make it easier to learn.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 11 years ago in reply to majorkuso

    The PSoC4 (programmable system-on-a-chip) includes an ARM Cortex M0 which is much faster than an Arduino.

    The PSoC4 Prototyping Kit ($4) is also much cheaper than an Arduino.

    Both systems have a free Integrated Development Environment. The PSoC IDE includes peripheral software drivers (including source code) for the system-on-a-chip.

    There is a new PSOC5 Prototyping Kit (for about $10) which is even more powerful (includes an ARM Cortex M3)

    I think the PSoC5 is a better kit because it includes a proper programmer/debugger (that can also be used with the PSoC4)

    There are lots of You Tube videos and the following projects provide great examples of how to implement real functionality:

    100 Projects in 100 Days

    100 projects in 100 days | Cypress

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 11 years ago in reply to majorkuso

    The PSoC4 (programmable system-on-a-chip) includes an ARM Cortex M0 which is much faster than an Arduino.

    The PSoC4 Prototyping Kit ($4) is also much cheaper than an Arduino.

    Both systems have a free Integrated Development Environment. The PSoC IDE includes peripheral software drivers (including source code) for the system-on-a-chip.

    There is a new PSOC5 Prototyping Kit (for about $10) which is even more powerful (includes an ARM Cortex M3)

    I think the PSoC5 is a better kit because it includes a proper programmer/debugger (that can also be used with the PSoC4)

    There are lots of You Tube videos and the following projects provide great examples of how to implement real functionality:

    100 Projects in 100 Days

    100 projects in 100 days | Cypress

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to dougw

    Caveat: PSoC4 and PSoC5 are great chips, but the PSoC Creator environment you need to design with them only runs on Microsoft Windows.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 11 years ago in reply to johnbeetem

    Good point John, I'm not a big fan of Windows, especially not 8.1, but there have always been orders of magnitude more programs that run on Windows than any other OS. If we refuse to use Windows, we have to give up a lot of choice and some productivity. The situation is improving steadily with more software running on other platforms and OS's, and deteriorating a bit with older software not running on new Windows and an ever increasing epidemic of malware, but everyone must weigh the trade-offs for their own requirements. For me, I just want to use the most productive and most powerful tools I can find, so I will have to keep a Windows machine around to run PSoC Creator and other key software - for a while. (I hear some people are running Creator in a virtual machine, but I have no Idea how effective that is)