Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum High Speed, High Current Op-amp
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 3 answers
  • Subscribers 505 subscribers
  • Views 2012 views
  • Users 0 members are here
  • electronics.
Related

High Speed, High Current Op-amp

michaelwylie
michaelwylie over 10 years ago

I'm looking for high speed (slew rate), high current op-amps. I'm aware of the external typologies that can be added to op-amps to increase the output current capability, but the component count starts to become daunting for my application. I'm trying to design a circuit to produce up to a 1.5 Amp current pulse to an optical device. The pulse will vary in width from 100 ns to 1000 ns depending upon the application. Rise/Fall less than 10 ns. I've been googling for a bit, and it seems to be exclusive. You can get either the high current, or the high slew rate. Any options would be great.

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 10 years ago +1 suggested
    Bi-FET reefers to amplifiers that use both bipolar and field-effect transistors in the same circuit. Early on, it was often a primitive mosfet driving a bipolar Q. This yielded a composite device that…
  • D_Hersey
    D_Hersey over 10 years ago +1
    The obvious superiority of a power mosfet over a power bipolar is saturation voltage. As a practical matter Si bipolars have a collector saturation of about half a volt. The mosfet conduction channel is…
  • D_Hersey
    D_Hersey over 10 years ago +1 suggested
    An emmiter-follower totempole at the gate of a power mosfet will work as well as a gate driver, at about a tenth of the cost.
  • D_Hersey
    0 D_Hersey over 10 years ago

    If you want a square-shaped pulse, you can use a bi-fet arrangement that consists of two inverting circuits in succession.  Then you attach a large-value resistor between the output and the input for a little positive feedback action.  The Schmidt trigger makes the output stage have crisper transitions than the circuit driving it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 10 years ago

    These guys are ever interesting.  They make Darlingtons that have BWs from DC to GHz.

     

    http://www.minicircuits.com/products/Amplifiers.shtml

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelwylie
    0 michaelwylie over 10 years ago in reply to D_Hersey

    I've given in. I need something like a push-pull configuration to get that negative bias.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelwylie
    0 michaelwylie over 10 years ago in reply to D_Hersey

    Can you elaborate on Bi-Fet?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 10 years ago

    Bi-FET reefers to amplifiers that use both bipolar and field-effect transistors in the same circuit.  Early on, it was often a primitive mosfet driving a bipolar Q.  This yielded a composite device that had the high Z-in of the mosfet and the ruggedness of the bipolar.  Connecting the drain of the mosfet to the collector of the bipolar was often possible, this made the mosfet current flow through the load as well as the bipolar.  This kept things relatively efficient.  In practice mosfet control terminals usually look like capacitors, which bipolars can be very good at slewing.

     

    Nowadays, since mosfets have gotten better, a mosfet is often the final.  A bipolar in common-emmiter mode is an inverter, providing 180 degrees of phase.  A mosfet in common source, driven by the switching bipolar also imposed 180 degrees of phase.  So the overall amplifier would have 360 degrees, equal to zero degrees (with a little delay) of phase.  The bipolar amplifier, on the left side, has an input resistor, typically, to convert the control potential into a current.  If we attach a large resistor from the final (mosfet) output all the way to the (bipolar) input, when the power switch we are constructing starts to turn on, load current (due to Q2) will make it turn on harder.  The on-to-off threshold has been biased away from the off-to-on threshold, thereby creating a Schmidt trigger.  This output side would not be good for audio, unless we are doing class D.  It makes for a very crisp pulse amp in terms of rise and fall times because those characteristics are not set by the driving pulse.  In a sense this output stage 'cleans up after' the controlling pulse.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 10 years ago

    The obvious superiority of a power mosfet over a power bipolar is saturation voltage.  As a practical matter Si bipolars have a collector saturation of about half a volt.  The mosfet conduction channel is resistor-like and can have an arbitrarily low saturation potential.  We can always make it half by shunting a like device, at the expense of doubling the gate capacitance.  This (bipolar fixed saturation potential) hardly matters if our bipolar Q's task is driving a mosfet's control terminal, as the mosfet gate threshold (we don't need to drive it all of the way low to turn it off) will always be greater than bipolar saturation potential and because the mosfet gate has very, very high resistance, so we don't have to worry about static dissipation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 10 years ago

    An emmiter-follower totempole at the gate of a power mosfet will work as well as a gate driver, at about a tenth of the cost.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<