Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum LPC2478-EVB KEIL linking errors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 502 subscribers
  • Views 325 views
  • Users 0 members are here
  • scatter file
  • lpc4357-evb
  • linker
Related

LPC2478-EVB KEIL linking errors

jobmenue
jobmenue over 10 years ago

I am getting linking errors with the by element14 supplied emWin demo software.

 

I know the basics (I would've thought I know more, but here we are) about linkers and compilers, but I just can't get this package to compile. It seems the scatter file is wrong, but where and why, I have no ******** clue. I have looked EVERYWHERE for a solution to the problem. It seems that it has something to do with the RAM or ROM memory, but I cannot figure out why or where.

 

Here's my build-output:

 

*** Using Compiler 'V5.06 update 2 (build 183)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'

Rebuild target 'LPC4357 Int. Flash'

assembling startup_LPC43xx.s...

compiling TSC_STMPE811.c...

compiling GUIConf.c...

compiling JOY_LPC43xx.c...

compiling I2C_LPC43xx.c...

compiling LCD_X_LPC4300.c...

compiling system_LPC43xx.c...

compiling LCDConf.c...

Driver\LCDConf.c(221): warning:  #177-D: function "delay" was declared but never referenced

  static void delay (int cnt) {

Driver\LCDConf.c: 1 warning, 0 errors

compiling GUI_X.c...

GUI_X.c(80): warning:  #223-D: function "SystemCoreClockUpdate" declared implicitly

  SystemCoreClockUpdate();

GUI_X.c: 1 warning, 0 errors

compiling main.c...

compiling GUIDEMO.c...

compiling GUIDEMO_Automotive.c...

compiling GUIDEMO_Bitmap.c...

compiling GUIDEMO_BarGraph.c...

compiling GUIDEMO_ColorBar.c...

compiling GUIDEMO_Conf.c...

compiling GUIDEMO_Cursor.c...

compiling GUIDEMO_Graph.c...

compiling GUIDEMO_Intro.c...

compiling GUIDEMO_Fading.c...

compiling GUIDEMO_ImageFlow.c...

compiling GUIDEMO_IconView.c...

compiling GUIDEMO_Listview.c...

compiling GUIDEMO_Resource.c...

compiling GUIDEMO_Skinning.c...

compiling GUIDEMO_Speed.c...

compiling GUIDEMO_Speedometer.c...

compiling GUIDEMO_Start.c...

compiling GUIDEMO_TransparentDialog.c...

compiling GUIDEMO_Treeview.c...

compiling GUIDEMO_VScreen.c...

compiling GUIDEMO_WashingMachine.c...

compiling lpc43xx_gpio.c...

compiling lpc43xx_timer.c...

compiling lpc43xx_lcd.c...

compiling GUIDEMO_ZoomAndRotate.c...

compiling lpc43xx_cgu.c...

compiling lpc43xx_rgu.c...

compiling lpc43xx_scu.c...

linking...

.\IntFlash\GUIDemo.axf: Warning: L6170W: Mapping symbol #19 '$t' in .bss(GUI_Curs1.o:8) identifies code, but is in a section not marked as executable.

.\IntFlash\GUIDemo.axf: Warning: L6170W: Mapping symbol #89 '$t' in .bss(GUI_SetAlpha.o:7) identifies code, but is in a section not marked as executable.

.\IntFlash\GUIDemo.axf: Warning: L6170W: Mapping symbol #42 '$t' in .bss(LISTVIEW.o:8) identifies code, but is in a section not marked as executable.

.\IntFlash\GUIDemo.axf: Warning: L6170W: Mapping symbol #31 '$t' in .bss(GUI_Timer.o:7) identifies code, but is in a section not marked as executable.

.\IntFlash\GUIDemo.axf: Warning: L6170W: Mapping symbol #7 '$t' in .bss(GUI__ManageCache.o:7) identifies code, but is in a section not marked as executable.

.\IntFlash\GUIDemo.axf: Warning: L6170W: Mapping symbol #19 '$t' in .bss(GUI__Alpha.o:7) identifies code, but is in a section not marked as executable.

.\IntFlash\GUIDemo.axf: Error: L6405E: No .ANY selector matches GUI_SetAlpha.o(.bss).

.\IntFlash\GUIDemo.axf: Error: L6405E: No .ANY selector matches GUI__ManageCache.o(.bss).

.\IntFlash\GUIDemo.axf: Error: L6405E: No .ANY selector matches GUI__Alpha.o(.bss).

.\IntFlash\GUIDemo.axf: Error: L6405E: No .ANY selector matches GUI_Timer.o(.bss).

.\IntFlash\GUIDemo.axf: Error: L6405E: No .ANY selector matches GUI_Curs1.o(.bss).

.\IntFlash\GUIDemo.axf: Error: L6405E: No .ANY selector matches LISTVIEW.o(.bss).

Not enough information to list image symbols.

Not enough information to list the image map.

Finished: 2 information, 6 warning and 6 error messages.

".\IntFlash\GUIDemo.axf" - 6 Error(s), 8 Warning(s).

Target not created.

Build Time Elapsed:  00:00:01

 

This is my scatter file:

 

; *************************************************************

; *** Scatter-Loading Description File generated by uVision ***

; *************************************************************

 

 

LR_IROM1 0x1A000000 0x00080000  {    ; load region size_region

  ER_IROM1 0x1A000000 0x00080000  {  ; load address = execution address

   *.o (RESET, +First)

   *(InRoot$$Sections)

   .ANY (+RO)

  }

  RW_IRAM1 0x10000000 0x00008000  {  ; RW data

   .ANY (+RW +ZI)

  }

  RW_IRAM2 0x20000000 0x00010000  {

   .ANY (+RW +ZI)

  }

 

  RW_RAM1 0x28000000 0x00800000  {

   * (VRAM, GUI_RAM, GUIDEMO_STACK, FS_RAM, IP_RAM, USB_RAM)

  }

}

 

Message was edited by: Moderator - removed profanity.